SNVS memory secured with tamper inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SNVS memory secured with tamper inputs

1,204 Views
juandiaz
Contributor II

Hello,

Is there a way to secure a SNVS_LP register or piece of memory from SNVS_LP to be zeroized in case of tamper input event?

Regards.

Tags (4)
0 Kudos
Reply
1 Reply

924 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Juan,

yes, it is possible using CAAM mndule. However this information is only provided under NDA. Please contact your DFAE or FAE to sign the NDA. They will provide this information directly to you


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply