Quick Help with GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Quick Help with GPIO

6,555件の閲覧回数
davidpeter
Contributor I

At a little bit of a lost here..  I'm not using MQX just some simple, I thought, GPIO writing and reading.  I seems to not clearly under stand the data sheet. 

example:

IOMUXC->SINGLE.PTC15 =  0x1D;  // set as input with 47K pull up on PTC15

rd = GPIO1->PDIR;       // read and bit 28 I think is PTC15 and it should be HIGH

what am I missing..

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

5,647件の閲覧回数
naoumgitnik
Senior Contributor V

Hello David,

Without going into details of your HW and SW, it is not enough to just enable a pull-up.

According to 'Chapter 5 Input/Output Multiplexer Controller (IOMUXC)' of 'Vybrid Reference Manual, Rev. 5, 07/2013', quite likely, you will also have to take care of the 'Buffer Enable' and 'Pull / Keep' fields (e.g. see the 'IOMUXC_PTA6 field descriptions' table).

Regards, Naoum Gitnik.

5,647件の閲覧回数
davidpeter
Contributor I

Naoum

Thanks, though the port is configured:

IOMUXC->SINGLE.PTC15 =  0x1D

which is 0x1D:

IOMUX_IBE_ENABLED

IOMUX_PUE_ENABLED

IOMUX_PKE_ENABLED

IOMUX_PUS_47KPUP

This config works OK with the two switches GPIO on the Tower VyBrid board  and the getting_started code for IAR.  I don't see any reference to Port Control. This does not mean I disagree with you guys.  I just don't see and code modifying the Port Control

0 件の賞賛
返信

5,647件の閲覧回数
billpringlemeir
Contributor V

It is possible that the boot ROM changes the PORT registers; especially if the GPIO is a boot config pin.  I looked in u-boot and the TimeSys Linux and didn't see a reference to the PORT registers there.  Maybe it is in the MQX code on the M4.  I didn't check that.  Are you using the same or different GPIOs as the tower switches in your bare metal version?

0 件の賞賛
返信

5,647件の閲覧回数
davidpeter
Contributor I

Bill,

We are using the switches plus some other GPIO.

0 件の賞賛
返信

5,647件の閲覧回数
billpringlemeir
Contributor V

You also need to turn on the clocks.  See pg670

  1. CCM_CCGR2[CG41] AIPS0-Slot73 Port A multiplexing control
  2. CCM_CCGR2[CG42] AIPS0-Slot74 Port B multiplexing control
  3. CCM_CCGR2[CG43] AIPS0-Slot75 Port C multiplexing control
  4. CCM_CCGR2[CG44] AIPS0-Slot76 Port D multiplexing control
  5. CCM_CCGR2[CG45] AIPS0-Slot77 Port E multiplexing control

These clocks are listed as disabled by the HAB/ROM (pg832, table 19-5).  u-boot seems to gate all the clocks on.  Check vybrid/lowlevel_init.S, for some start code.

0 件の賞賛
返信

5,647件の閲覧回数
billpringlemeir
Contributor V

The PORT CONTROL module must be configured to an interrupt.  See section 7.3 of the manual.  Is PTC the same as GPIO1?  I think it should be GPIO2 for PTC.  Ie, GPIO0-4 gives PT[A-E].

Edit: PTC15 is very weird naming.  It is actully RGPIO-60 (60-32=28), so it is GPIO-1 bit 28.  Section 8.11.1.1 GPIO Mapping gives an overview of all the PTxNN mappings to the GPIO values.  This can be very confusing.  The PTxNN are only used for pin naming.

0 件の賞賛
返信

5,647件の閲覧回数
naoumgitnik
Senior Contributor V

Good point, Bill!

"7.3.1 General-purpose input

The logic state of each pin is available via the Port Data Input registers, provided the pin is configured for a digital function and the corresponding Port Control and Interrupt module is enabled.

The Port Data Input registers return the synchronized pin state after any enabled digital filter in the Port Control and Interrupt module. The input pin synchronizers are shared with the Port Control and Interrupt module, so that if the corresponding Port Control and

Interrupt module is disabled, then synchronizers are also disabled."

Interestingly enough, "This config works OK with the two switches GPIO on the Tower VyBrid board" for the discussion originator; IMO, something changed in the settings, and quite likely what you mentioned.

Regards, Naoum Gitnik.

0 件の賞賛
返信