Problem with EDGE interrupt detection and generation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problem with EDGE interrupt detection and generation

跳至解决方案
7,035 次查看
pivkluka
Contributor III

Hi,

We have a GPIO pin defined as input and interrupt on that pin is configured as falling edge. When we plug the clock/signal generator/or just simple DC voltage to that GPIO pin we get some extra interrupts on rising edge.

As you can see on images:

CLOCK is the input signal to that GPIO

TEST is the pin that toggles on every interrupt it receives.

DATA  you can just ignore it on some pictures.

We are running Windows Embedded Compact 7.

What we did so far and didn't help:

1. Enable schmitt trigger - does nothing

2. Enable digital filters - does nothing

3. Change PIN - same thing happens

4. Change PORT - same thing happens

5. Frequency of clock signal doesn't effect the issue

6. Use another GPIO as interrupt source - same thing happens

7. Used the rising edge interrupt - same thing happens

We tried on VF6XX and VF5XX

Regards,
Luka

tek00009.pngtek00002.png

tek00009.pngtek00008.pngtek00007.png

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
6,215 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
7 回复数
6,216 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
6,224 次查看
richard_stulens
NXP Employee
NXP Employee

Hi Luka,

Is this topic still open?

I went over the images again but I cannot think of any other reasons for this behavior.

If it is still open, please check if there are effectively no glitches and also check if the interrupt came from the expected source.

Best regards,

Richard


0 项奖励
回复
6,224 次查看
richard_stulens
NXP Employee
NXP Employee

Hi Luka,

It looks as if there is a pretty serious glitch on the clock signal and this is seen as clock edge.

glitch.png

These inputs are very fast. Even a glitch of less than 1ns can be picked up.

All images seem to have some sort of noise, but I cannot tell if tere are actually glitches.

There is a filter option on the GPIOs. Maybe you can use that to filter out glitches.

Best will be to make sure signals are clean, without ringing. Use lower drive strength and/or edge rate on outputs where possible.

This will also help reduce EMC emissions.

Best regards,

Richard


0 项奖励
回复
6,224 次查看
pivkluka
Contributor III

Hi,

As I did write the filter does not help at all.

We used many diferent signals ( it just looks like there are glitches but if you zoom in signal there is nothing that shouldnt be there )

We even tryed only connecting 1 GPIO as output to another GPIO as input to interrupt source and toggle the 1st GPIO and we still get to many errors.

0 项奖励
回复
6,224 次查看
richard_stulens
NXP Employee
NXP Employee

Hi Luka,

I'm not sure how we can help with this issue.

The interrupts must come form somewhere. If it is not from glitches then there must be some other source.

In the first image, where I thought there was a glitch,  the toggle occurs when there is no transition on the clock, so it is not even triggering on the wrong edge.

I also checked with a colleague of mine about the filter on the GPIO. He confirmed the digital filter should work on the GPI inputs, so if it makes no difference it's probably not glitches, but then it must come from some other source or from a different input pin.

Here are a few suggestions to try/check:

Do you verify in the ISR that the interrupt was from the input that you expect before toggling the output pin?

Are any other interrupts enabled? What happens when you do not toggle the input at all? Are there still interrupts?

Regards,

Richard

6,225 次查看
pivkluka
Contributor III

Hi,

This is the only interrupt, And when we dont have a clock signal there is no interrupts happening.

Regards,

Luka

0 项奖励
回复
6,225 次查看
juhaaaltonen
Contributor I

I also got the impression that the interrupts are received OK, but there is something funny in the output, although the signal looks too clean to be output HW problem. It looks like the "interrupt counter" does something wrong.

0 项奖励
回复