Linux init overwrite iomux register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux init overwrite iomux register

1,846件の閲覧回数
Nouchi
Senior Contributor II

Hello,

At Linux boot time, after mvf_board_init(), IOMUXC_PTB8 is overwritten in my back by something between "io scheduler cfq" registration and console initialization.

Any ideas? It makes me insane.....

Emmabnuel

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

1,648件の閲覧回数
timesyssupport
Senior Contributor II

Hi Emmanuel,

What hardware were you using when you encountered this issue? Can you reproduce on the Vybrid Tower kit?

Thanks,

Timesys Support

0 件の賞賛
返信

1,648件の閲覧回数
Nouchi
Senior Contributor II

Hello,

I'm using my own design based on TWR-VF65GS10 for most part, and autoEVB for Ethernet part. In my case PTB8 is used as FTM1 chan0 capture mode. I set  IOMUX with 0x00101201, and at the end I get 0x0000219e.

At this moment, I don't have enough time to dig deeper, I will do it in few weeks, as workaround, M4 MQX application rewrite IOMUXC, dirty but it works.

Emmanuel

0 件の賞賛
返信

1,649件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you attend this case?

0 件の賞賛
返信