LPDDR2 Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,806件の閲覧回数
jonpartee
Contributor I

What do the TINIT, TINIT3, TINIT4, TINIT5 in the DDR_CR02-DDR_CR05 Correspond to in reference to LPDDR2 data sheet.  The latest reference manual has little/no information on this.  Not all of the LPDDR2 datasheets label the INIT times the same.

Jon

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
2,340件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Yes, seems the manual is lacking from that information.

TINIT: Defines the DRAM initialization delay, in memory clocks.(time required for memory clocks to be started and stabilized before clock enable becomes active)

TINIT3: Defines the number of memory clocks required from CKE assertion to memory reset. (this parameter only applies when the controller is configured for LPDDR2)

TINIT4: Defines the number of memory clocks required from memory reset to an MRR command (this parameter only applies when the controller is configured for LPDDR2)

TINIT5: Defines the maximum number of memory clocks required from memory reset to initialization complete (this parameter only applies when the controller is configured for LPDDR2)


AlejandroSierra, you may be interested on this...

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,340件の閲覧回数
ioseph_martinez
NXP Employee
NXP Employee

Yes, seems the manual is lacking from that information.

TINIT: Defines the DRAM initialization delay, in memory clocks.(time required for memory clocks to be started and stabilized before clock enable becomes active)

TINIT3: Defines the number of memory clocks required from CKE assertion to memory reset. (this parameter only applies when the controller is configured for LPDDR2)

TINIT4: Defines the number of memory clocks required from memory reset to an MRR command (this parameter only applies when the controller is configured for LPDDR2)

TINIT5: Defines the maximum number of memory clocks required from memory reset to initialization complete (this parameter only applies when the controller is configured for LPDDR2)


AlejandroSierra, you may be interested on this...

0 件の賞賛
返信