LCD Rotate Display 180 Degrees

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LCD Rotate Display 180 Degrees

4,672件の閲覧回数
carlovalgocela
Contributor III

Good Day

I'm trying to integrate LCD  NHD-5.0-800480TF-ATXL into our system.

The display is now working. However due to hardware and physical location of the LCD I need to rotate the display 180 degrees.

I tried using updating files as mentioned in this discussionRotate the 3.5 inch LCD screen to 180 degree.

The result is it will only rotate the logo and when i run some GUI applications or display images it will revert back.

Any ideas what needs to be updated to successfully rotate the screen?

Thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

3,966件の閲覧回数
timesyssupport
Senior Contributor II

Hello carlovalgocela and karinavalencia,

As noted in the same thread you have in Timesys Support, it appears the framebuffer driver does not support rotation in it's default state; an application or framework, such as Qt or X must be leveraged, unless the driver is customized to rotate. If this is a hard requirement, please contact Timesys Sales to discuss a dedicated engineer to integrate.

Thank you,

Timesys Support

3,966件の閲覧回数
Nouchi
Senior Contributor II

Hi Carlo,

If you use QT4 library, you can rotate screen with 'transformed" option like that : YourApp -qws -display transformed:rot180:1.

Regards,

Emmanuel

3,966件の閲覧回数
carlovalgocela
Contributor III

Thanks. That is one of our option.

My concern if i am not using QT and need the lcd rotated 180 degrees

0 件の賞賛
返信

3,966件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help here?

0 件の賞賛
返信