GPU GC355 not responding and it got stuck.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPU GC355 not responding and it got stuck.

2,479件の閲覧回数
sathishkumarsig
Contributor II

Hi,

How I can ensure whether the GPU gc355 in vybrid processor is executed all of the commands in the command buffer(0x400CF500)?

In Vybrid_Reference_Manual_F_Series_-_Rev_3.pdf, it is mentioned that the GPU will generate the interrupt after all the IDLE bits goes high and INTR enabled.

If i consider the idle register(0x400CF004) status, sometimes it is having 0x7ffff7fe instead of 0x7fffffff/e.

The Clock Control Register (0x400C_F000) having 0x00040100 instead of 0x00070100 for longtime.

Is there is any error status register to find out the reason why the commands are not get processed?

Please support.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,243件の閲覧回数
timesyssupport
Senior Contributor II

Hello

The Vybrid Tower platform currently does not have GPU support. It seems you are looking at an older revision of the reference manual - the current revision (VYBRIDRM) is here, with no reference to the gc355 chip:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=VF6xx&fpsp=1&tab=Documentation_Tab

Regards,

Timesys Support

2,243件の閲覧回数
sathishkumarsig
Contributor II

Hi Timesys Support,

Thanks for your reply. The Micro chip placed in the Faraday EVB is PVF522R3K1CMK4.

0 件の賞賛
返信

2,243件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信