GPU GC355 not responding and it got stuck.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPU GC355 not responding and it got stuck.

1,822 次查看
sathishkumarsig
Contributor II

Hi,

How I can ensure whether the GPU gc355 in vybrid processor is executed all of the commands in the command buffer(0x400CF500)?

In Vybrid_Reference_Manual_F_Series_-_Rev_3.pdf, it is mentioned that the GPU will generate the interrupt after all the IDLE bits goes high and INTR enabled.

If i consider the idle register(0x400CF004) status, sometimes it is having 0x7ffff7fe instead of 0x7fffffff/e.

The Clock Control Register (0x400C_F000) having 0x00040100 instead of 0x00070100 for longtime.

Is there is any error status register to find out the reason why the commands are not get processed?

Please support.

标签 (1)
0 项奖励
回复
3 回复数

1,586 次查看
timesyssupport
Senior Contributor II

Hello

The Vybrid Tower platform currently does not have GPU support. It seems you are looking at an older revision of the reference manual - the current revision (VYBRIDRM) is here, with no reference to the gc355 chip:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=VF6xx&fpsp=1&tab=Documentation_Tab

Regards,

Timesys Support

1,586 次查看
sathishkumarsig
Contributor II

Hi Timesys Support,

Thanks for your reply. The Micro chip placed in the Faraday EVB is PVF522R3K1CMK4.

0 项奖励
回复

1,586 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 项奖励
回复