NXP MCAL Package

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP MCAL Package

2,064件の閲覧回数
Vinaymsn
Contributor I

Hi Team,

For S32K3xx series NXP controller - We are planning to buy the NXP MCAL Package for Autosar Project.

The BSW Modules Configuration is done via Vector Davinci Configurator Tool.

1. Can NXP Mcal package be integrated into Davinci configurator directly using the Third-Party setup which vector supports?? and MCAL modules can be configured and generated?

2. Does Eb Tresos Tool is used for MCAL configuration .. Is it a separate License we need to buy for EB Tresos for configuration or is it part of NXP Package.?

 

Thanks for your support

 

Thanks

Vinay

0 件の賞賛
返信
1 返信

1,998件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vinaymsn,

I apologize for the late reply, there was an issue with the tracker tool, and the ticket never got assigned. However, I can see this is the same question you posted to the support case internally, so in order to avoid any confusion, I will keep supporting you through your case.

Best regards,
Julián

0 件の賞賛
返信