NXP MCAL Package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP MCAL Package

2,170 Views
Vinaymsn
Contributor I

Hi Team,

For S32K3xx series NXP controller - We are planning to buy the NXP MCAL Package for Autosar Project.

The BSW Modules Configuration is done via Vector Davinci Configurator Tool.

1. Can NXP Mcal package be integrated into Davinci configurator directly using the Third-Party setup which vector supports?? and MCAL modules can be configured and generated?

2. Does Eb Tresos Tool is used for MCAL configuration .. Is it a separate License we need to buy for EB Tresos for configuration or is it part of NXP Package.?

 

Thanks for your support

 

Thanks

Vinay

0 Kudos
Reply
1 Reply

2,104 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vinaymsn,

I apologize for the late reply, there was an issue with the tracker tool, and the ticket never got assigned. However, I can see this is the same question you posted to the support case internally, so in order to avoid any confusion, I will keep supporting you through your case.

Best regards,
Julián

0 Kudos
Reply