u4gm:Diamond Matron Location in Last Epoch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u4gm:Diamond Matron Location in Last Epoch

1,816 Views
1fuhd
Contributor I

Diamond Matrons in Last Epoch are formidable enemies known for their healing abilities and challenging combat mechanics. They primarily appear in the Maj’elka region during the Divine Era, making this area the best place to locate and farm them efficiently.

Primary Locations
Players can find Diamond Matrons in three key story zones within Maj’elka:Temple Rooftops,Upper Temple and Lower Temple.
Among these, the Upper Temple is widely regarded as the premier farming spot. It contains three consistent Diamond Matron spawn points located close to the waypoint, allowing for quick and efficient runs. After clearing the Matrons, players can reset the zone by teleporting to another waypoint and returning, which respawns enemies and enables repeated farming without delay.

Farming in Monolith Echoes
Diamond Matrons also spawn in certain Monolith Echoes, including:
The Age of Winter,The Stolen Lance,Ending The Storm and Reign Of Dragons.

However, farming in Monoliths is less reliable due to randomized enemy spawns and the procedural nature of the maps. Some prophecies require killing Diamond Matrons specifically within Monoliths, so players may need to explore these Echoes and hope for their appearance. This method is slower and more passive compared to the targeted farming possible in the Upper Temple.

Combat Tips
Diamond Matrons possess three main abilities:
1. Light Beam: A beam of light that follows the player, which can be dodged.
2. Light Wave: A shockwave attack dealing damage.
3. Healing Hand: Heals themselves and nearby allies when low on health.

The healing ability can be particularly frustrating if the Matron is surrounded by other enemies. To counter this, it’s effective to either eliminate nearby enemies first or lure the Diamond Matron away from groups to prevent healing. Notably, while casting Light Beam, the Matron cannot perform other attacks, providing a valuable window to deal damage.

For more information and updates about Last Epoch ,you can follow u4gm.

Tags (1)
0 Kudos
Reply
0 Replies