Grow a Garden 2 Movement Guide: How to Walk Faster Instantly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Grow a Garden 2 Movement Guide: How to Walk Faster Instantly

1,315 Views
JordanBlair
Contributor I

If you have spent any decent amount of time grinding in Roblox Grow a Garden 2, you already know the pain of moving at a snail's pace. When a rare mutation event triggers and you need to secure those seeds before anyone else, or when a greenhouse thief is trying to swipe your hard work, every second counts. Navigating those massive plots can feel like a massive chore if you are stuck at base speed.

Fortunately, you do not have to settle for the default walk cycle. Whether you want a permanent passive buff, a quick consumable sprint, or a hilarious physics glitch to launch yourself across the map, here is exactly how to maximize your movement speed instantly.

Permanent Speed Boosts: The Bunny Stack Strategy

If you want a reliable, permanent upgrade to your baseline speed, you need to dive into the game’s pet system. The undisputed kings of passive speed are Bunny pets.

Each active Bunny pet you equip gives you a flat +5 Walk Speed bonus. When you first start out, the game allows you to equip up to three pets simultaneously. By stacking a full squad of three Bunnies right off the bat, you instantly gain a +15 speed bonus, completely changing how fast you cover ground.

Getting your hands on these little speed demons comes down to two main methods:

  • Keep an eye on the map. Bunnies randomly spawn in the world, and you can buy them outright for 20,000 Sheckles.

  • Try your luck at the gacha. You can hatch them from a Common Egg, which features a pretty generous 30% hatch rate.

Once you have your squad assembled, you can push your passive movement caps even higher by applying Pet Toys to your equipped Bunnies, which further enhances their baseline stats.

Temporary Speed Boosts: Mushrooms and Teleportation

Sometimes you do not need permanent speed; you just need an immediate, aggressive burst of velocity to chase down an intruder or sprint to the shop before a timer runs out. That is where gear and consumables come into play.

  • Speed Mushrooms: For a quick fix, head over to the Gear Store and pick up some Speed Mushrooms for 1,500 Sheckles. Consuming one gives you a massive velocity boost for a short duration, perfect for clutch situations.

  • Teleporter Wrench: If you have some cash to burn, save up 18,000 Sheckles for the Teleporter Wrench at the Gear Store. This legendary item lets you completely bypass the act of walking altogether by letting you instantly blink a short distance forward.

The Fun Alternative: The Celestberry Physics Glitch

If you are low on Sheckles but still want to move at hyper-speed, you can exploit a structural physics glitch carried over from the original game. It takes a little bit of setup, but the results are ridiculous.

First, you need to grow a massive plant. A Celestberry works perfectly for this, though any high-tier, heavy plant like Bamboo will do. To super-size it, group multiple Basic and Advanced Sprinklers closely around the plant until it grows to a massive weight, ideally around 12 to 14 kg.

Once your mega-plant is fully grown, harvest it and equip it directly into your hand.

To trigger the launch, switch your camera view into first-person. Face completely away from your intended destination, hold down your backward movement key, turn on Shift Lock, and continuously tap your jump key. Because of the bizarre collision geometry of the giant fruit interacting with your character model, the game physics will break, violently flinging you backward across the map at insane speeds.

Whether you choose to build a dedicated Bunny army, stock up on mushrooms, or fling yourself across the zone with a giant berry, there is no reason to suffer through slow walk speeds anymore. Pick the method that fits your budget and start zooming around your plot.

0 Kudos
Reply
0 Replies