ServoMotor S3010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ServoMotor S3010

1,086 Views
thibaultferrant
Contributor I

Hello,

At every start of our system, we notice that the ServoMotor isn't at the same position with the same command signal. So we can't find the command signal to go straight. Is it normal or not? Our ServoMotor is it break?

Thanks for your answer.

0 Kudos
2 Replies

815 Views
rolfschlagenhaf
NXP Employee
NXP Employee

Hi Thibault,

something you might want to check: Sometimes the servo (or anything mechanically moved by it) might hit a mechanical limitation. This can deposition the lever (yellow plastic part) on the servo's axle. The servo's axle has a big momentum. In software you could limit the min/max positions to avoid running into mechanical limitations. But during powering up or flashing the system, these software limits don't apply yet and the servor can drive the mechanics still into physical limits with quite some momentum. Same for the motors, by the way. It's a good idea to power the motor control board only when proper software limitation is running. De-powering it while flashing or resetting of the controller board might help.

Of course your problem can also have another cause like e.g. a broken servo.

Rolf

815 Views
thibaultferrant
Contributor I

We are going to test with tightening the screw of the lever and disconnect it before each restart. Thanks for the advise, i'll come back to tell you the result.

0 Kudos