This is with great pleasure that we have 19 teams qualified for the NXP Cup EMEA finals that will be held at the Fraunhofer IIS in Erlangen on 16-17 April 2018.
The qualified teams are (17 from Universities and 2 from High Schools):
Country | University/Company | Team | Model |
Germany | Deggendorf Institute of Technology | Die 2 Lustigen 3 | Alamak |
The K-Team | Model C | ||
FH Bielefeld University of Applied Science | BiAxial | Model C | |
Tryhard | Model C | ||
Nuremberg Institute of Technology Georg Simon Ohm | Ohm_Racer_3 | Model C | |
Greece | Technological Educational Institute of Piraeus | Athlos | Alamak |
Morocco | University Mundiapolis | Mac | Model C |
Sigma | Model C | ||
Poland | Wroclaw University of Technology | Syndergy | Alamak |
Synergia | Alamak | ||
Romania | Technical University of Iasi | ACDT | Alamak |
University of Craiova | FasTech | Alamak | |
UCC | Model C | ||
Slovakia | Stredna priemyselna skola elektrotechnicka Piestany | Prima | HS Model C |
Spirit | HS Model C | ||
Slovak Technological University from Bratislava | Elita | Model C | |
Switzerland | Haute Ecole ARC Ingénierie | ARCar2 | Model C |
ARCar3 | Model C | ||
Ukraine | ONPU - Odessa National Polytechnic University | Wonderbolts | Model C |
All the information regarding the logistics for the EMEA finals can be found at https://community.nxp.com/docs/DOC-335342
Students and professors attending the event will be contacted directly by the NXP organising team.
已解决! 转到解答。