Taplinx iOS read Desfire EV2 fails on authentication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Taplinx iOS read Desfire EV2 fails on authentication

3,829件の閲覧回数
sh4
Contributor II

self.desFireEV2?.authenticate(withCardKeyNo: 1, withAuthenticationType: .AES, withAuthKeyType: .AES128, withCommandSetForAuth: .ISO, withAuthkey: "AES_KEY".hexStringToData()!, onCompletion: { [unowned self] success in
print(success)
}

on authentication, the app crashes with untraceable records, even in crashlaytics not getting the traces. 

-----------------------------
Debug Print
-----------------------------

Response received : AFD7AF4F60A515551FD8332907BDA43BAA

DES Session Key Before - <ComNxpNfclibDefaultimplKeyData: 0x1056e7340>

AES Session Key Data After - <ComNxpNfclibDefaultimplKeyData: 0x1056e7340>

AES Session Key Data Array After - {length = 16, bytes = AES_KEY}

------ AES, {length = 16, bytes = 0xd7af4f60a515551fd8332907bda43baa}, {length = 16, bytes = 0xAES_KEY}, {length = 16, bytes = 0x00000000000000000000000000000000} ------

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,796件の閲覧回数
sh4
Contributor II

Debug executable option already disabled. 

0 件の賞賛
返信

3,742件の閲覧回数
Florian_Mikulik
NXP Employee
NXP Employee

Hi!

As you probably know, all documentation from MIFARE DESFire is available only under NDA, so we can not discuss any details here. However, i see a descrepancy here, that might solve the problem:

you are using the authenticate command,  withCommandSetForAuth: .ISO and try to use AES keys. This seems not to fit together. MIFARE DESFire supports several authentication methods, each resulting in different secure messaging modes and each using different keys ONLY (e.g. AuthenticateISO only can be used with 3DES keys. Its crucial to use the correct combination of key and authentication. All of this can be found in the datasheet of MIFARE DESFire. In case of deeper support needed, please open a ticket with our online support team that enables us also to discuss topics protected by NDA.

 

Thanks,

Br,

Florian 

Customer Application Support Engineer - Gratkorn - Austria
0 件の賞賛
返信

3,651件の閲覧回数
sh4
Contributor II

Hi Florian,

I checked with both withCommandSetForAuth: .ISO, and .native but in both cases getting crash that are untraceable.

Can you please share the link of the data sheet?


0 件の賞賛
返信

3,638件の閲覧回数
Florian_Mikulik
NXP Employee
NXP Employee

hello,

 

For the datasheet, please log in at nxp.com, and then request secure file access for your account. This will only be possible if an active NDA with nxp is in place. If you do not have an active NDA, please request one in the support section of nxp.com.

Only once this is in place, the datasheet can be provided to your account.

 

regards,

Florian

Customer Application Support Engineer - Gratkorn - Austria
0 件の賞賛
返信

3,787件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir,

Thank you for using our community.

This is NXP's customer support, would you mind sharing if the crashing only happens when trying to read the DESFire card with authentication? 

Can you read an NDEF of the card? It is also important to know what procedure are you following for configuring the card. The more information we have about your setup the better we can assist.

Best Regards,
Fabian
0 件の賞賛
返信

3,764件の閲覧回数
sh4
Contributor II

in other functions, I am getting success, such as selectApplication, getApplicationId and others. but while authenticating, getting untraced crashes. 

  func tagReaderSession(_ session: NFCTagReaderSession, didDetect tags: [NFCTag]) {

    guard let tag = tags.first else { return }

 

    // Connect to the tag

    session.connect(to: tag) { [weak self] error in

      guard let self = self else { return }

      if let error = error {

        session.invalidate(errorMessage: "Failed to connect: \(error.localizedDescription)")

        return

      }

      switch tag {

 

      case .miFare(let mifare):

        let reader = TL_IOSNFCReader(uid: mifare.identifier, historicalBytes: mifare.historicalBytes!)

        self.handler = TapLinxApduHandler(reader: reader)

        self.handler?.delegate = self

        

        self.tagManager = TLLibraryManager.shared()

self.tagManager?.setApduHandlerWithApduHandler(self.handler)

var desfireWrapper = TL_DESFireWrapper(libraryManager: self.tagManager!)

        print(desfireWrapper)

        desfireWrapper.setCommandSet(.Native)

         desFireEV2 = self.tagManager?.getDESFireEV2Instance()

self.desFireEV2?.selectApplication(withAppID: Int32("0")!) { success in

          print("selectApplication: success \(success)")

        }

 

        self.desFireEV2?.getApplicationIDs() { success in

          print("Get application IDs: success \(success)")

        }

 

        self.desFireEV2?.selectApplication(withAppID: Int32(applicationId)!) { success in

          print("selectApplication: success \(success)")

        }

 

        self.desFireEV2?.getKeyVersion(forKeyNumber: 1) { value, success in

          print("Get key version: success \(success)")

        }

 

        self.desFireEV2?.getFileIDs() { value, success in

          print("Get file IDs: success \(success)")

        }

 

        self.desFireEV2?.authenticate(withCardKeyNo: 1, withAuthenticationType: .AES, withAuthKeyType: .AES128, withCommandSetForAuth: .ISO, withAuthkey: aesKeyData, onCompletion: { [weak self] success in

          print("authenticate: success", success)

          if success {

            self?.desFireEV2?.readData(withFileNo: 1, withOffset: 0, withLength: 4) { data, success in

              print("readDataWithFileNo: success \(success) - data = \(data)")

            }

          }

        })
}

func apduExchange(withByteArray apduData: Data) -> TL_TagAPDUResponse? {

    var dataToreturn = Data()

    let semaphore = DispatchSemaphore(value: 0)

 

    mtag?.sendMiFareCommand(commandPacket: apduData) { data, error in

      dataToreturn = data

      semaphore.signal()

    }

 

    _ = semaphore.wait(timeout: .now() + 3.0)

    let tl = TL_TagAPDUResponse(responseData: dataToreturn, tag: tagInfo)

    return tl

  }

0 件の賞賛
返信

3,818件の閲覧回数
Octopussy
Contributor I

I had the same issue. Please see the answer in the following post: https://community.nxp.com/t5/TapLinx-SDK-TagWriter-and/Taplinx-iOS-app-reading-Desfire-EV2/td-p/2013...

The short answer is: Disable Debugging when running the app in Xcode.

  1. Select the scheme that you are using to run the application
  2. Edit Scheme
  3. In the Info Tab, uncheck the Debug executable option.

 

0 件の賞賛
返信