TagWriter - my datasets .twdb restore backup error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TagWriter - my datasets .twdb restore backup error

1,788件の閲覧回数
peku
Contributor II

Hi, I am trying to restore backup of my datasets in NXP TagWriter 6.1.0 - bookmarks prepared for NTAG213 with uid and interaction counter mirroring.

I save .twdb file but when I load it back its not correctly loaded into TagWriter.

 

{"cardTypeString":"NTAG213","gpioStatusEnabled":false,"gpioStatusOffset":-1,"mByteOffsetForCounter":3,"mByteOffsetForTT":-1,"mByteOffsetForUID":0,"mCounterOffset":-1,"mEnableCounter":true,"mEnableEncryptedFileDataMirroring":false,"mEnableNTAG413DNASDMAndMirroring":false,"mEnableNTAG413DNASUMMessage":false,"mEnableNTAG424DNASDMMirroring":false,"mEnableSDMReadCounterLimit":false,"mEnableTT":false,"mEnableUID":true,"mEncryptionDataLength":-1,"mEncrytionDataOffset":-1,"mMACInputOffset":-1,"mMACOffset":-1,"mNTag22xEnableMirrorConfiguration":false,"mNtag22xEnableNfcCounter":false,"mPICCOffset":-1,"mPageOffsetForCounter":5,"mPageOffsetForTT":-1,"mPageOffsetForUID":17,"mSdmCounterRetrievalKey":-1,"mSdmFileReadAccessKey":-1,"mSdmMetaReadAccessRight":-1,"mSdmReadCounterLimit":[0,0,0],"mTTCustomMessageEnabled":false,"mTTMessage":[0,0,0,0],"mTTStatusOffset":-1,"mUIDOffset":-1,"ttStatus":0}

This is part of data inside exported twdb file. Clearly it is supposed to be NTAG213 but after loading back to app its completly messed up (see picture).

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,773件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @peku,

Hope you are doing well.

Please, consider that TagWriter app is intended for testing purposes.

After importing a dataset backup, it should be merged as expected into My datasets. The screen shown in your picture is the default screen for editing/configuring the mirror features, but your dataset should actually have remained unchanged.

Regards,
Eduardo.

0 件の賞賛
返信

1,758件の閲覧回数
peku
Contributor II

Hi,

The issue is definitely a bug—it genuinely doesn't work. When you load a backup back into TagWriter, it disables the UID and Interaction Counter, and it also changes the tag type from NTAG213 to NTAG210.

I discovered this while trying to find a workaround, because importing from a CSV file doesn't work either. It's impossible to import a CSV for NTAG213, and the UID mirror and Interaction Counter features also don't function correctly.

 

0 件の賞賛
返信

1,744件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I will try to report this behavior; however, I cannot guarantee that a workaround or fix will be released. Please, consider that this application is intended for testing purposes. I truly apologize for the inconvenience.

Regarding the CSV file, perhaps you may find some useful information in this Community post: Error "Not valid NDEF records found" when trying to select a CSV in TagWriter for Android - NXP Comm....

Regards,
Eduardo.

0 件の賞賛
返信