TagWriter - my datasets .twdb restore backup error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TagWriter - my datasets .twdb restore backup error

1,804 Views
peku
Contributor II

Hi, I am trying to restore backup of my datasets in NXP TagWriter 6.1.0 - bookmarks prepared for NTAG213 with uid and interaction counter mirroring.

I save .twdb file but when I load it back its not correctly loaded into TagWriter.

 

{"cardTypeString":"NTAG213","gpioStatusEnabled":false,"gpioStatusOffset":-1,"mByteOffsetForCounter":3,"mByteOffsetForTT":-1,"mByteOffsetForUID":0,"mCounterOffset":-1,"mEnableCounter":true,"mEnableEncryptedFileDataMirroring":false,"mEnableNTAG413DNASDMAndMirroring":false,"mEnableNTAG413DNASUMMessage":false,"mEnableNTAG424DNASDMMirroring":false,"mEnableSDMReadCounterLimit":false,"mEnableTT":false,"mEnableUID":true,"mEncryptionDataLength":-1,"mEncrytionDataOffset":-1,"mMACInputOffset":-1,"mMACOffset":-1,"mNTag22xEnableMirrorConfiguration":false,"mNtag22xEnableNfcCounter":false,"mPICCOffset":-1,"mPageOffsetForCounter":5,"mPageOffsetForTT":-1,"mPageOffsetForUID":17,"mSdmCounterRetrievalKey":-1,"mSdmFileReadAccessKey":-1,"mSdmMetaReadAccessRight":-1,"mSdmReadCounterLimit":[0,0,0],"mTTCustomMessageEnabled":false,"mTTMessage":[0,0,0,0],"mTTStatusOffset":-1,"mUIDOffset":-1,"ttStatus":0}

This is part of data inside exported twdb file. Clearly it is supposed to be NTAG213 but after loading back to app its completly messed up (see picture).

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,789 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @peku,

Hope you are doing well.

Please, consider that TagWriter app is intended for testing purposes.

After importing a dataset backup, it should be merged as expected into My datasets. The screen shown in your picture is the default screen for editing/configuring the mirror features, but your dataset should actually have remained unchanged.

Regards,
Eduardo.

0 Kudos
Reply

1,774 Views
peku
Contributor II

Hi,

The issue is definitely a bug—it genuinely doesn't work. When you load a backup back into TagWriter, it disables the UID and Interaction Counter, and it also changes the tag type from NTAG213 to NTAG210.

I discovered this while trying to find a workaround, because importing from a CSV file doesn't work either. It's impossible to import a CSV for NTAG213, and the UID mirror and Interaction Counter features also don't function correctly.

 

0 Kudos
Reply

1,760 Views
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I will try to report this behavior; however, I cannot guarantee that a workaround or fix will be released. Please, consider that this application is intended for testing purposes. I truly apologize for the inconvenience.

Regarding the CSV file, perhaps you may find some useful information in this Community post: Error "Not valid NDEF records found" when trying to select a CSV in TagWriter for Android - NXP Comm....

Regards,
Eduardo.

0 Kudos
Reply