t2081 pcie Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

t2081 pcie Issue

3,629 Views
arumilli
Contributor I

I am working on T2081 custom board. After booting Linux and run the commanddmesg | grep -i pci i got some error.  How to resolve these issues.

I am using t2081 evk qds devicetree

root@t2081qds:/sys/bus/pci/devices# dmesg | grep -i pci
[ 0.318064] Found FSL PCI host bridge at 0x0000000ffe270000. Firmware bus number: 0->0
[ 0.324595] PCI host bridge /pcie@ffe270000 ranges:
[ 0.342076] /pcie@ffe270000: PCICSRBAR @ 0xff000007
[ 0.345589] setup_pci_atmu: end of DRAM c0000000
[ 0.350059] /pcie@ffe270000: Setting PCI inbound window greater than memory size
[ 0.357009] EDAC PCI0: Giving out device to module MPC85xx_edac controller mpc85xx_pci_err : DEV ffe270000.pcie (INTERRUPT)
[ 0.366699] MPC85xx_edac acquired irq 23 for PCI Err
[ 0.370315] MPC85xx_edac PCI err registered
[ 0.373240] platform ffe270000.pcie:pcie@0: Invalid size 0xfffff9 for dma-range
[ 0.402817] PCI: Probing PCI hardware
[ 0.405168] fsl-pci ffe270000.pcie: PCI host bridge to bus 0000:00
[ 0.409963] pci_bus 0000:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000- 0xffff])
[ 0.417613] pci_bus 0000:00: root bus resource [mem 0xc40000000-0xc4fffffff] (bus address [0xe0000000-0xefffffff])
[ 0.426654] pci_bus 0000:00: root bus resource [bus 00]
[ 0.430563] pci_bus 0000:00: busn_res: [bus 00] end is updated to ff
[ 0.431298] pci 0000:00:00.0: [1957:0838] type 01 class 0x0b2000
[ 0.432030] pci 0000:00:00.0: [Firmware Bug]: reg 0x10: invalid BAR (can't size)
[ 0.439082] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]
[ 0.442327] pci 0000:00:00.0: supports D1 D2
[ 0.442331] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 0.443943] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[ 0.451882] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 0.455836] pci 0000:00:00.0: bridge window [io 0x10000-0x10fff]
[ 0.455914] pci 0000:00:00.0: bridge window [mem 0x00000000-0x000fffff]
[ 0.456111] pci 0000:00:00.0: bridge window [mem 0x00000000-0x000fffff 64bit pref]
[ 0.456411] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[ 0.456417] pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01
[ 0.456523] PCI 0000:00 Cannot reserve Legacy IO [io 0x10000-0x10fff]
[ 0.456595] pci 0000:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]
[ 0.462256] pci 0000:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]
[ 0.468342] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.472026] pci 0000:00:00.0: bridge window [io 0x10000-0x1ffff]
[ 0.476950] pci 0000:00:00.0: bridge window [mem 0xc40000000-0xc4fffffff]
[ 0.482812] pci_bus 0000:00: resource 4 [io 0x10000-0x1ffff]
[ 0.482816] pci_bus 0000:00: resource 5 [mem 0xc40000000-0xc4fffffff]
[ 0.482819] pci_bus 0000:01: resource 0 [io 0x10000-0x1ffff]
[ 0.482823] pci_bus 0000:01: resource 1 [mem 0xc40000000-0xc4fffffff]
[ 0.482824] PCI: Probing PCI hardware done
[ 1.516030] PCI: CLS 0 bytes, default 64
[ 1.594297] aer 0000:00:00.0:pcie02: service driver aer loaded
[ 2.024312] ehci-pci: EHCI PCI platform driver
root@t2081qds:/sys/bus/pci/devices#

Thanks and Regards,

Ravindra

0 Kudos
Reply
4 Replies

3,128 Views
arumilli
Contributor I

Hello,

Any Update on This regarding PCI issue in T2081 board

Thanks,

Ravindra.

0 Kudos
Reply

3,607 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Please validate your RCW configuration ( According to the SERDES configuration you selected), you can also try to test the pcie device under u-boot to se if the device is recognized with the pci commands. 

Your Linux complains that it cannot assign the amount of memory the peripheral connected to the PCIe wants, please share complete log file in .txt format.

0 Kudos
Reply

3,573 Views
arumilli
Contributor I

Hi,

Here i attached the full log file

0 Kudos
Reply

3,123 Views
arumilli
Contributor I
Hello,
Is there any update regarding the PCI issue?
0 Kudos
Reply