fsl_memcpy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,531件の閲覧回数
michayardeny
Contributor III

1. I reviewed the fsl_memcpy procudure in the SDK v1.6 for e5500 my question if there is available results of the memcpy_test?

2. I want to run memcpy test  with the SDK how do I do it ?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,298件の閲覧回数
Pavel
NXP Employee
NXP Employee

This procedure is not procedure from kernel source.

Look at the Section 3.3.19 in NXP SDK 2.0-1703 documentation (FAQ). Find the following:"How do I install source code, modify source code and rebuild u-boot/kernel" and "How to add a pre-built ppc binary into the rootfs"


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,299件の閲覧回数
Pavel
NXP Employee
NXP Employee

This procedure is not procedure from kernel source.

Look at the Section 3.3.19 in NXP SDK 2.0-1703 documentation (FAQ). Find the following:"How do I install source code, modify source code and rebuild u-boot/kernel" and "How to add a pre-built ppc binary into the rootfs"


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,298件の閲覧回数
michayardeny
Contributor III

May be I was wrong in my question but at the same build QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/work/ppce5500-fsl-linux/libppc/git-r0/git/fsl-opt-lib/tests/memcpy/memcpy_test.c

e5500 is the architecture of t1040rdb. So the question is precisely if that all build with this BSP how can I activate the test.

Best Regards

Micha 

0 件の賞賛
返信
3,298件の閲覧回数
Pavel
NXP Employee
NXP Employee

There are no similar procedures in the SDK v1.6 for e5500. For example see the T1040rdb kernel source using the following path:

QorIQ-SDK-V1.6-20140619-yocto/build_t1040rdb_release/tmp/work/t1040rdb-fsl-linux/linux-qoriq-sdk/3.12-r0/git


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信