codewarrior for T4240

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior for T4240

ソリューションへジャンプ
5,103件の閲覧回数
ericskullerud
Contributor II

Hi,

I've looked over the download selections at the FreeScale CodeWarrior site and can't figure out which version is the correct one for supporting installation of QCVS, so that I can edit the RCW for the T4240.

That is all I need CodeWarrior for - we are targeting VxWorks and have no interest in CodeWarrior beyond RCW edits.

Can anyone here point me to the correct download?

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
4,699件の閲覧回数
addiyi
NXP Employee
NXP Employee

For eclipse 4.4.x it is mandatory to by installed the Freescale Updater attached, before QCVS installation.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,699件の閲覧回数
addiyi
NXP Employee
NXP Employee

Hi,

You have three possibilities:

1. Install over eclipse using update site;

2. Install over CodeWarrior for Power Architerctures;

3. Install during CodeWarrior for ARMv7 installation;

Please refer to QCVS installation guide.

Adrian

0 件の賞賛
返信
4,699件の閲覧回数
ericskullerud
Contributor II

Hi,

My response to  your 3 options:

1) using update site in the installation guide (at link you included - thank you) results in:

  You don't have permission to access /lgfiles/updates/Eclipse/QCVS/ on this server.

Can you please provide the correct link (I have Eclipse 4.4.1 Luna installed)?

2) I don't see a download for a CodeW for Power Architecture - can you please provide a link?

3) We are targeting T4240 PPC architecture - how is it ARMv7 install will work correctly for our target?

Thank you.

0 件の賞賛
返信
4,700件の閲覧回数
addiyi
NXP Employee
NXP Employee

For eclipse 4.4.x it is mandatory to by installed the Freescale Updater attached, before QCVS installation.

Adrian

0 件の賞賛
返信
4,699件の閲覧回数
addiyi
NXP Employee
NXP Employee

1. http://freescale.com/lgfiles/updates/Eclipse/QCVS

2. CodeWarrior for PA

3. QCVS is common for both PA and ARMv7

Adrian

0 件の賞賛
返信