Writing to NOR Flash while executing from it in T1024

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing to NOR Flash while executing from it in T1024

1,267件の閲覧回数
veerendranathj
Contributor III

Is it possible to write/program to NOR flash while executing code from it?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
ufedor
NXP Employee
NXP Employee

This is hardly possible without specially designed code which should be allocated and locked in a cache.

0 件の賞賛
返信