What is the compatible Power Architecture Processor(COP) probe tip for T1024?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the compatible Power Architecture Processor(COP) probe tip for T1024?

3,416 Views
veerendranathj
Contributor III

As far as I know all the things(both hardware and software) we need to buy from freescale to set up complete development and debugging environment for T1024RDB.

1) CodeWarrior Development Studio for Power Architecture Technology (Eclipse) v10.5 Developer License (software)

2) CodeWarrior TAP (hardware )

3) Power ArchPitecture processor ( COP ) Probe Tip for CodeWarrior TAP (hardware )

let me know if I am missing anything.

But T1024 is not there in the list devices supported by "Power Architecture processor ( COP ) Probe Tips" then how can we flash or debug the board and what is the compatible probe tip for T1024?

Labels (1)
0 Kudos
Reply
5 Replies

2,966 Views
addiyi
NXP Employee
NXP Employee

COP Probe Tip for CodeWarrior TAP (CWH-CTP-COP-YE) is the probe tip targeted for T1024. You didn't miss anything from your list. All these should be enough for flashing or/and debugging your T1024 board.

Adrian

0 Kudos
Reply

2,966 Views
veerendranathj
Contributor III

But T1024 is not listed in the supported devices of COP Probe Tip for CodeWarrior TAP (CWH-CTP-COP-YE)?

Reference:

Power Architecture processor for CodeWarrior|Freescale

0 Kudos
Reply

2,966 Views
addiyi
NXP Employee
NXP Employee

All T1 series support COP as Jtag interface. Take a look on T1024RDBRM​ and on T1024RM.

Adrian

0 Kudos
Reply

2,966 Views
veerendranathj
Contributor III

Thanks... I thought it won't support due to lack of information in official webpage of COP Probe Tip(CWH-CTP-COP-YE). It would be good if the information in the webpage will be updated correctly.

Can we use Lauterbach LA-3794(QorIQ 64-Bit devices compatible debugger) for debugging from Codewarrior IDE?

what are the options available debugging from Codewarrior IDE other than Codewarrior TAP?

what are the standalone debuggers(i.e only for debugging, In case we use open source GCC toolchain instead of Code Warrior IDE) available for QorIQ T1024 debugging?

0 Kudos
Reply

2,966 Views
sinanakman
Senior Contributor III

Hi Veerendranath

We use BDI3000 and it supports T devices

including T1020.

Hope this helps

Sinan Akman

0 Kudos
Reply