T4240RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240RDB

2,788件の閲覧回数
bogdantanasa
Contributor II

Hi,

Is it possible to connect a SATA hard disk to the T4240RDB board? What kind of cabling is needed?

ラベル(1)
5 返答(返信)

2,529件の閲覧回数
ufedor
NXP Employee
NXP Employee

Socket for the SATA Data Cable is present on-board.

SATA Power cable is provided by the RDB's PSU.

0 件の賞賛
返信

2,529件の閲覧回数
bogdantanasa
Contributor II

Thank you!

Can you also tell me if the board is delivered with DDR3 memory or one has to buy it separately? If yes, which kind of memory is delivered?

0 件の賞賛
返信

2,529件の閲覧回数
ufedor
NXP Employee
NXP Employee

The RDB is equipped with 3 x 4GB UDIMMs.

The RDB documentation is available at:

QorIQ T4240 Reference Design Board|NXP

0 件の賞賛
返信

2,529件の閲覧回数
bogdantanasa
Contributor II

I am wondering if this is really true (i.e. 12GB of memory).

In the T4240RDBQS.pdf it says that 3 DIMMS slots are supported (2 GB per DIMM) while in T4240RDBFS.pdf it says:

"Three unbuffered DDR3 240-pin uDIMM modules with ECC (72-bit bus), 6 GB memory, 1866 MT/s data rate"

which would suggest that the memory is pre-installed.

The confusing arises from the fact that T4240RDBQS.pdf does not give the impression that the memory is pre-installed.

Thanks.

0 件の賞賛
返信

2,529件の閲覧回数
ufedor
NXP Employee
NXP Employee

You are right.

I'm sorry for the issue with the memory size.

This is the real board booting log shows:

DRAM:  Initializing....using SPD

Detected UDIMM 9JSF25672AZ-2G1K1

Detected UDIMM 9JSF25672AZ-2G1K1

Detected UDIMM 9JSF25672AZ-2G1K1

4 GiB left unmapped

6 GiB (DDR3, 64-bit, CL=13, ECC on)

       DDR Controller Interleaving Mode: 3-way 4KB

The memory surely is pre-installed.

The issue was caused by the RDB board documentation issue (QorIQ T4240 Reference Design Board Quick Start, Rev. 2) where the log is:

DRAM: Initializing....using SPD

Detected UDIMM 18JSF51272AZ-1G9K1

Detected UDIMM 18JSF51272AZ-1G9K1

Detected UDIMM 18JSF51272AZ-1G9K1

10 GiB left unmapped

12 GiB (DDR3, 64-bit, CL=13, ECC on)

DDR Controller Interleaving Mode: 3-way 4KB

DDR Chip-Select Interleaving Mode: CS0+CS1