T4240 rman stop working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240 rman stop working

1,466 Views
Timmy1
Contributor I

Hi!

      I used the t4240's DPAA to transfer data between the rapidio and the 10-gigabit network. But occasionally there are problems. rman was unable to process the received data and the software did not report any errors. But when I looked at the registers associated with rman, I found that the Message Manager Status Register (MMSR) had a different value than when it was working normally. OHWC (Open hardware contexts) is 0x10. I tried to change the GEN value of the MMRCAR register to 0x18 maximum. However, the fault persists. The OHWC still reaches the maximum value 0x18. How can I avoid this situation? Open hardware contexts are fully occupied.

                                                                                                                                       Thanks a lot!

0 Kudos
Reply
2 Replies

1,444 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to A-009006 in chip errata.

0 Kudos
Reply

1,438 Views
Timmy1
Contributor I
Thanks a lot for helping! But where could I download the document? I didn't find it anywhere.
0 Kudos
Reply