T4240 data rate ratios

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T4240 data rate ratios

3,177件の閲覧回数
davidcchung
NXP Employee
NXP Employee

Why can I not set all the DDR data rate ratios that the reference manual says are supported by the RCW “MEM_PLL_RAT” field bits 10-15?

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

2,973件の閲覧回数
Saul_Salazar
NXP Employee
NXP Employee

There is a footnote in the T4240 reference manual that states “Not all ratios are supported due to frequency restrictions. Refer to the hardware specifications for the supported frequencies."


Hope it helps

0 件の賞賛
返信

2,973件の閲覧回数
addiyi
NXP Employee
NXP Employee

Do you try to use QCVS? Or what is your scenario?

Adrian

0 件の賞賛
返信