T4240 DFloat calculated performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240 DFloat calculated performance

1,322 Views
sunzhengyu
Contributor I

Which document has a description of the floating point capability index for the T4240 Processor?

Labels (1)
0 Kudos
Reply
1 Reply

1,140 Views
alexander_yakov
NXP Employee
NXP Employee

Please look e6500 Core Reference Manual, Chapter 10 "Execution Timing"

Table 10-4 shows "instruction latencies". In this table you can see two columns - "latency" and "repeat time". For example, for floating point multiply instruction "fmul" there will be 1 and 7. This means each instruction takes 7 clocks, but you can issue these instructions one-by-one at every clock in pipelined mode and have a result at every cycle.

Direct link to e6500 Core Reference Manual:

http://www.nxp.com/assets/documents/data/en/reference-manuals/E6500RM.pdf 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply