T2081 DDR3L on-board initialisation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2081 DDR3L on-board initialisation

1,043 次查看
ioxos
Contributor I

WE are using a T2081 with on-board 4x DDR3L 4Gb  256Mx16/ MT41K256M16-1600 , so we do not have on-board  SPD. Can you supply us  data to fill the dimm_param_s data structure used by UBOOT ?

Best rgards

标签 (1)
0 项奖励
回复
1 回复

799 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK supports the T208xQDS and T208sRDB boards. U-boot for these boards uses SPD for DDR configuring.

See the t208xrdb.zip file in the attachment.

Find the following line in the ddr.h file:

static const struct board_specific_parameters udimm0[] = {

This structure contains the following parameters:

n_ranks, datarate_mhz_high, rank_gb, clk_adjust, wrlvl_start, wrlvl_ctl_2, wrlvl_ctl_3.

Look at the T1023RDB setting in the t102xrdb.h file. Find the CONFIG_SYS_DDR_RAW_TIMING in this file. This setting provides do not use SPD for DDR configuring. See the  t102xrdb.h and ddr_t102xrdb.c files for the T102sRDB board from u-boot. See the ddr_raw_timing procedure in the ddr_t102xrdb.c file.

Use similar method for your T2081 board.

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复