T2080RDB aurora connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080RDB aurora connection

1,011 Views
metinmert_deniz
Contributor I

Hello, We are trying to use Aurora interface on our T2080RDB. I am wondering to how can we do physical connection of Aurora interface. T2080RDB board does not have its Aurora connector on it. I read that,SerDes pins can be used for connection,in the community. Is it possible or could you suggest any connector/adaptor exists for Aurora?

0 Kudos
Reply
1 Reply

853 Views
ufedor
NXP Employee
NXP Employee

> SerDes pins can be used for connection

SerDes 2 lanes 4 & 5 can be configure as Aurora interface.

Please refer to the QorIQ T2080 Reference Manual, Table 19-1. SerDes Lanes Assignments and Multiplexing.

Aurora connector is present on the T2080QDS-PA.

T2080RDB can't be modified to use Aurora connection.

0 Kudos
Reply