T2080RDB MAC Addy's

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,971件の閲覧回数
elsasnow
Contributor II

Am I missing something about how MAC's are assigned to T2080RDB ETH4 and ETH5?

In Linux:

ifconfig fm1-mac3 192.168.0.22

ifconfig

fm1-mac3 Link encap:Ethernet  HWaddr 00:04:9f:03:c9:8c

Connected to ETH4 on front panel

Label on this port on T2080RDB has last # of MAC as 8D (Port next to USB stack).

Is there a chance the board is simply mislabeled with the MAC stickers?

Is this table correct regarding assignment of front panel ports to u-boot/Linux?

Capture.PNG

I have two RDB's doing this same thing.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,760件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Label on this port on T2080RDB has last # of MAC as 8D (Port next to USB stack).

Please provide photo(s) of the stickers on your board.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,761件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Label on this port on T2080RDB has last # of MAC as 8D (Port next to USB stack).

Please provide photo(s) of the stickers on your board.

0 件の賞賛
返信
2,760件の閲覧回数
elsasnow
Contributor II

From the QS guide, it appears ETH4 and ETH5 are swapped to front panel.

Capture.JPG

Here are our MAC labels (note routing to front panel.  Eth4 is going ot ETH5 front panel

P7180125.JPG

A closer view:

P7180127.JPG

Our front panel as assigned by actual MAC's

P7180128.JPG

And a followup question:

Are ETH4 and ETH5 the only ports on this board that can run at 1Gbps?  Can Eth0, Eth1, Eth2, or Eth3 be configured to run at 1Gbps instead of 10Gbps, or does the PHY clock dictate that they are always at 10?

0 件の賞賛
返信
2,760件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Are ETH4 and ETH5 the only ports on this board that can run at 1Gbps?

Yes.

0 件の賞賛
返信