T2080 VID question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 VID question

1,033件の閲覧回数
xiaopengma
Contributor I

I have reviewed T4240 Data Sheet and T2080 Data Sheet,found that they may be woking on the same VID mechanism.

There is a Note in T4240 Data Sheet:

"9. If VID is known at initial start-up, set VDD=VID else if VID is not known at initial start-up, set VDD to 1.025V and change it

immediately, to VDD=VID after reading VID at the beginning of booting."

Does this Note apply to T2080?

ラベル(1)
0 件の賞賛
返信
1 返信

929件の閲覧回数
ufedor
NXP Employee
NXP Employee

Yes.

The same functioning is described in the T2080 QorIQ Integrated Multicore Communications Processor data sheet, 4.2.1 Voltage ID (VID) controllable supply.

0 件の賞賛
返信