T2080 VID question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T2080 VID question

1,508 次查看
xiaopengma
Contributor I

I have reviewed T4240 Data Sheet and T2080 Data Sheet,found that they may be woking on the same VID mechanism.

There is a Note in T4240 Data Sheet:

"9. If VID is known at initial start-up, set VDD=VID else if VID is not known at initial start-up, set VDD to 1.025V and change it

immediately, to VDD=VID after reading VID at the beginning of booting."

Does this Note apply to T2080?

标签 (1)
0 项奖励
回复
1 回复

1,404 次查看
ufedor
NXP Employee
NXP Employee

Yes.

The same functioning is described in the T2080 QorIQ Integrated Multicore Communications Processor data sheet, 4.2.1 Voltage ID (VID) controllable supply.

0 项奖励
回复