T2080 SerDes Clock Signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080 SerDes Clock Signals

1,455 Views
paulagarcía-mor
Contributor I

I am working with a T2080 device and I need some help to understand the voltage level of some signals.

According to the datasheet of the microprocessor, the input voltage range of every SerDes signal, including clocks, is GND to SVDD (which is 1V).

But, in the reference design board, the serdes clock signals that go to the T2080 inputs (SD1_REFCLK1_P, SD_REFCLK1_N...) have a higher voltage level (2V5/3V3).

How can it be possible?  Is the input voltage range higher for clock signals than for the rest of the serdes signals?

Thank you in advance.

Paula

Labels (1)
0 Kudos
Reply
1 Reply

1,339 Views
alexander_yakov
NXP Employee
NXP Employee

According to the datasheet of the microprocessor, the input voltage range of every SerDes signal, including clocks, is GND to SVDD (which is 1V).

Please look T2080 device datasheet, Section 3.19.2.2 "SerDes reference clock receiver characteristics". There are 50 Ohm on-chip termination and AC decoupling. Actual voltage amplitude depends on how clock driver is coupled with clock input.

But, in the reference design board, the serdes clock signals that go to the T2080 inputs (SD1_REFCLK1_P, SD_REFCLK1_N...) have a higher voltage level (2V5/3V3).

The chip U23 (PI3PCIE3212), which is powered from 3.3V, is only switch chip, and the fact that this switch is powered from 3.3V does not mean output signals are 3.3V. The chip U48 (IDT9FGV0641) is powered from 1.8V, and there is also output termination.


Have a great day,
Alexander,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply