T1042 onboard ethernet testing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 onboard ethernet testing

1,087 Views
qammarabbas
Contributor IV

Hi NXP Team,

I have designed a custom board using T1042. I am using 2 PHYs with the ethernet interface. Currently, i am in testing phase of my board. How can i test whether the ethernet interface is working or not? Is there any protocol or software for this purpose? Any information regarding the query will be appreciated. 

Tags (1)
1 Reply

992 Views
Pavel
NXP Employee
NXP Employee

Use u-boot for data loading via TFTP. If there is no problem during data loading under u-boot, load Linux image (kernel, root file system and .dtb file).

 

There are a lot test programs under Linux. For example, see the following:

https://elinux.org/images/d/df/Understanding_Embedded_Linux_Benchmarking_Using_Kernel_Trace_Analysis...

 

or

 

https://spindance.com/test-automation-embedded-part-1/

 

Look at also the following document:

https://www.embeddedartists.com/sites/default/files/support/com/Interface_Testing_on_iMX_Developers_...

 

Use this document as example for board testing.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------