T1042 - DDR Controller Commad Signal Timings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1042 - DDR Controller Commad Signal Timings

2,018 Views
EmbEng
Contributor III

Hi, We are trying to bringup DDR3L discrete RAMs on our custom board. We modified our RCW to set DDR clock frequency to 533MHz. We created a default QCVS DDR3 validation project and ran validation tests. All tests are failing by giving following errors:

Error configuring the target! - DDR initialization failed: D_INIT was not cleared by hardware

We verified signal routing, CLK, CKE and checked signals on probes on all command signals (RAS, CAS, WE, BA, Address etc.) used during DRAM init. However, we noticed two following abnormalities in the signals:

1.  CKE was following init sequence but once it goes high it does not come to low (although CKE_PLS bits are set to use 4 clocks)

2.  Command signals (we tested RAS and CAS) are being asserted for 3~4 clock cycles i.e 7~8 ns when running on 533MHz (although 1T timing is set in DDR controller settings). Please checkout the attached snapshot of RAS signal during init sequence.

Can someone confirm why T1042/DDR-controller is driving these signals with such behavior? Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
7 Replies

1,753 Views
ufedor
NXP Employee
NXP Employee

Points to check:

1) RESET to the DDR SDRAM chips is applied correctly

2) DDR controller DQ mapping settings correspond to the schematics

0 Kudos
Reply

1,753 Views
EmbEng
Contributor III

Thanks ufedor‌.

1) RESET to the DDR SDRAM chips is applied correctly

DDR Chips' reset is asserted with PORESET_B signal and de-asserted with HRESET signal. Although the board is meeting minimum timing requirement of CKE (i.e. CKE must remain low for at least 500us after chips' RESET is de-asserted), the CKE signal remains low for at least 2.5 seconds and then goes high continuously.

2) DDR controller DQ mapping settings correspond to the schematics

Our routing is done on 1-1 basis on all 10 chips, so mapping settings also seem to be correct as shown below:

DQ_Mappings.PNG

DQ_Mappings_schematic.PNG

0 Kudos
Reply

1,753 Views
ufedor
NXP Employee
NXP Employee

What are the DDR controller registers values?

0 Kudos
Reply

1,753 Views
EmbEng
Contributor III

Please check following settings. Our board has 2 chipselects but we are testing for 1 chipselect only just to troubleshoot the issue:

   # DDR_SDRAM_CFG 
   mem i:0xFE008110 = [value_of 0x67240000] 
   # CS0_BNDS 
   mem i:0xFE008000 = [value_of 0x010001FF] 
   # CS1_BNDS 
   mem i:0xFE008008 = [value_of 0x020002FF] 
   # CS2_BNDS 
   mem i:0xFE008010 = [value_of 0x0300033F] 
   # CS3_BNDS 
   mem i:0xFE008018 = [value_of 0x0340037F] 
   # CS0_CONFIG 
   mem i:0xFE008080 = [value_of 0x80014402] 
   # CS1_CONFIG 
   mem i:0xFE008084 = [value_of 0x00010202] 
   # CS2_CONFIG 
   mem i:0xFE008088 = [value_of 0x0202] 
   # CS3_CONFIG 
   mem i:0xFE00808C = [value_of 0x0202] 
   # CS0_CONFIG_2 
   mem i:0xFE0080C0 = [value_of 0x00] 
   # CS1_CONFIG_2 
   mem i:0xFE0080C4 = [value_of 0x00] 
   # CS2_CONFIG_2 
   mem i:0xFE0080C8 = [value_of 0x00] 
   # CS3_CONFIG_2 
   mem i:0xFE0080CC = [value_of 0x00] 
   # TIMING_CFG_3 
   mem i:0xFE008100 = [value_of 0x000B0000] 
   # TIMING_CFG_0 
   mem i:0xFE008104 = [value_of 0x4044000C] 
   # TIMING_CFG_1 
   mem i:0xFE008108 = [value_of 0xB3BE3A75] 
   # TIMING_CFG_2 
   mem i:0xFE00810C = [value_of 0x0030D116] 
   # DDR_SDRAM_CFG_2 
   mem i:0xFE008114 = [value_of 0x00401810] 
   # DDR_SDRAM_MODE 
   mem i:0xFE008118 = [value_of 0x00061A40] 
   # DDR_SDRAM_MODE_2 
   mem i:0xFE00811C = [value_of 0x00080000] 
   # DDR_SDRAM_MODE_2 
   mem i:0xFE00811C = [value_of 0x00080000] 
   # DDR_SDRAM_MODE_2 
   mem i:0xFE00811C = [value_of 0x00080000] 
   # DDR_SDRAM_MODE_3 
   mem i:0xFE008200 = [value_of 0x00] 
   # DDR_SDRAM_MODE_4 
   mem i:0xFE008204 = [value_of 0x00] 
   # DDR_SDRAM_MODE_5 
   mem i:0xFE008208 = [value_of 0x00] 
   # DDR_SDRAM_MODE_6 
   mem i:0xFE00820C = [value_of 0x00] 
   # DDR_SDRAM_MODE_7 
   mem i:0xFE008210 = [value_of 0x00] 
   # DDR_SDRAM_MODE_8 
   mem i:0xFE008214 = [value_of 0x00] 
   # DDR_SDRAM_MD_CNTL 
   mem i:0xFE008120 = [value_of 0x00000000] 
   # DDR_SDRAM_INTERVAL 
   mem i:0xFE008124 = [value_of 0x1034040D] 
   # DDR_DATA_INIT 
   mem i:0xFE008128 = [value_of 0xDEADBEEF] 
   # DDR_SDRAM_CLK_CNTL 
   mem i:0xFE008130 = [value_of 0x02800000] 
   # DDR_INIT_ADDR 
   mem i:0xFE008148 = [value_of 0x00000000] 
   # DDR_INIT_EXT_ADDR 
   mem i:0xFE00814C = [value_of 0x00000000] 
   # TIMING_CFG_4 
   mem i:0xFE008160 = [value_of 0x01] 
   # TIMING_CFG_5 
   mem i:0xFE008164 = [value_of 0x03401400] 
   # DDR_ZQ_CNTL 
   mem i:0xFE008170 = [value_of 0x89080600] 
   # DDR_WRLVL_CNTL 
   mem i:0xFE008174 = [value_of 0x8655F60D] 
   # DDR_SR_CNTR 
   mem i:0xFE00817C = [value_of 0x00000000] 
   # DDR_WRLVL_CNTL_2 
   mem i:0xFE008190 = [value_of 0x00] 
   # DDR_WRLVL_CNTL_3 
   mem i:0xFE008194 = [value_of 0x00] 
   # DDR_ERR_DISABLE 
   mem i:0xFE008E44 = [value_of 0x00] 
   # DDR_ERR_INT_EN 
   mem i:0xFE008E48 = [value_of 0x1D] 
   # DDR_ERR_SBE 
   mem i:0xFE008E58 = [value_of 0x00010000] 
   # DDRCDR_1 
   mem i:0xFE008B28 = [value_of 0x80040000] 
   # DDRCDR_2 
   mem i:0xFE008B2C = [value_of 0x01] 
   # DDR_SDRAM_CFG_3 
   mem i:0xFE008260 = [value_of 0x00] 
   # TIMING_CFG_6 
   mem i:0xFE008168 = [value_of 0x00] 
   # TIMING_CFG_7 
   mem i:0xFE00816C = [value_of 0x00] 
   # TIMING_CFG_8 
   mem i:0xFE008250 = [value_of 0x00] 
   # DESKEW_CNTL 
   mem i:0xFE0082A0 = [value_of 0x00] 
   # DQ_MAP0 
   mem i:DDRmc1_DQ_MAP0_ADDR = [value_of 0x06106104] 
   # DQ_MAP1 
   mem i:DDRmc1_DQ_MAP1_ADDR = [value_of 0x84184184] 
   # DQ_MAP2 
   mem i:DDRmc1_DQ_MAP2_ADDR= [value_of 0x06106104] 
   # DQ_MAP3 
   mem i:DDRmc1_DQ_MAP3_ADDR = [value_of 0x84184000] 
   # DDR_SDRAM_MODE_9 
   mem i:0xFE008220 = [value_of 0x00] 
   # DDR_SDRAM_MODE_10 
   mem i:0xFE008224 = [value_of 0x00] 
   # DDR_SDRAM_MODE_11 
   mem i:0xFE008228 = [value_of 0x00] 
   # DDR_SDRAM_MODE_12 
   mem i:0xFE00822C = [value_of 0x00] 
   # DDR_SDRAM_MODE_13 
   mem i:0xFE008230 = [value_of 0x00] 
   # DDR_SDRAM_MODE_14 
   mem i:0xFE008234 = [value_of 0x00] 
   # DDR_SDRAM_MODE_15 
   mem i:0xFE008238 = [value_of 0x00] 
   # DDR_SDRAM_MODE_16 
   mem i:0xFE00823C = [value_of 0x00] 
   # DDR_SDRAM_RCW_3 
   mem i:0xFE0081A0 = [value_of 0x00] 
   # DDR_SDRAM_RCW_4 
   mem i:0xFE0081A4 = [value_of 0x00] 
   # DDR_SDRAM_RCW_5 
   mem i:0xFE0081A8 = [value_of 0x00] 
   # DDR_SDRAM_RCW_6 
   mem i:0xFE0081AC = [value_of 0x00] 
   #Delay before enable 
   wait 500 
   #DDR_SDRAM_CFG 
   mem i:0xFE008110 = [value_of 0xE7240000]
0 Kudos
Reply

1,753 Views
ufedor
NXP Employee
NXP Employee

Please provide the processor connection schematics for inspection as searchable PDF.

To do that it will be convenient to create a Technical Case:

1)    open www.nxp.com
2)    Select "Support" -> "All Support Options"
3)    Click "Go to Tickets"
4)    Log in with your NXP login and password
5)    On the "Group, Create and View your support cases" page press "+ Add a new case" to start the process.

0 Kudos
Reply

1,753 Views
EmbEng
Contributor III

I have a case already opened regarding DDR bringup issue. Should I add these details to that case or open a new case for you?

0 Kudos
Reply

1,753 Views
ufedor
NXP Employee
NXP Employee

Please add the details to the Case.

0 Kudos
Reply