T1040: chip selects issue in uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

T1040: chip selects issue in uboot

1,445 次查看
gouravjain
Contributor IV

Hi,

I want to enable some more chip selects from IFC controller. Tried to make changes in u-boot also, but its got hanged.

Here are the changes made by me,

1) T104xRDB.h

#define CONFIG_SYS_RAYCOM1_BASE    0xFF900000

#define CONFIG_SYS_RAYCOM1_BASE_PHYS       (0xf00000000ull | CONFIG_SYS_RAYCOM1_BASE)

#define CONFIG_SYS_CSPR3_EXT    (0xf)

#define CONFIG_SYS_CSPR3        (CSPR_PHYS_ADDR(CONFIG_SYS_RAYCOM1_BASE_PHYS) \

                                | CSPR_PORT_SIZE_8 \

                                | CSPR_MSEL_GPCM \

                                | CSPR_V)

#define CONFIG_SYS_AMASK3       IFC_AMASK(64*1024)

#define CONFIG_SYS_CSOR3        0x0

/* RAYCOM1 Timing parameters for IFC CS2 */

#define CONFIG_SYS_CS3_FTIM0            (FTIM0_GPCM_TACSE(0x0e) | \

                                        FTIM0_GPCM_TEADC(0x0e) | \

                                        FTIM0_GPCM_TEAHC(0x0e))

#define CONFIG_SYS_CS3_FTIM1            (FTIM1_GPCM_TACO(0x0e) | \

                                        FTIM1_GPCM_TRAD(0x1f))

#define CONFIG_SYS_CS3_FTIM2            (FTIM2_GPCM_TCS(0x0e) | \

                                        FTIM2_GPCM_TCH(0x0) | \

                                        FTIM2_GPCM_TWP(0x1f))

#define CONFIG_SYS_CS3_FTIM3            0x0

2) tlb.c

#ifdef CONFIG_SYS_RAYCOM1_BASE

        SET_TLB_ENTRY(1, CONFIG_SYS_RAYCOM1_BASE, CONFIG_SYS_RAYCOM1_BASE_PHYS,

                      MAS3_SW|MAS3_SR, MAS2_I|MAS2_G,

                      0, 14, BOOKE_PAGESZ_256K, 1),

#endif

3) law.c

#ifdef CONFIG_SYS_RAYCOM1_BASE_PHYS

         SET_LAW(CONFIG_SYS_RAYCOM1_BASE_PHYS, LAW_SIZE_64K, LAW_TRGT_IF_IFC),

#endif

pls let me know where im doing wrong. Any more configuration is required???

--

Gourav

标签 (1)
0 项奖励
回复
3 回复数

1,153 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Gourav Jain,

What kind of device is configured at IFC CS2? How do you decide IFC Timing parameters for this device?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,153 次查看
gouravjain
Contributor IV

Hi Yiping,

Issue got resolved. It was there because of IFC clock, which was higher than expected for end device.

thanks for you interest in my post..

--

Gourav

0 项奖励
回复

1,153 次查看
hareeshp
Contributor II

Hi gourav jain,

   Could you please share what you had tried to solve this issue?. Because we are also facing the same issue.

0 项奖励
回复