T1022 Serdes Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1022 Serdes Configuration

1,649件の閲覧回数
swatig
Contributor I

I want to connect T1022 in PCIe x4 configuration and SGMII on other ports. So, I have to use 0x40 Serdes configuration. 0x40 configuration has one PCIe x2 , one PCIe x4 and SGMII on other ports. But even X1 PCIe is sufficient for my requirement. So, is it possible that I connect only lane 0 of the PCIe x2 port to the end point device and run PCIe in x1 mode ? Or is it necessary to connect both the lanes of PCIe port even for PCIe x1 to work?

ラベル(1)
0 件の賞賛
返信
1 返信

1,642件の閲覧回数
r8070z
NXP Employee
NXP Employee

According to the PCIe specs it is possible connect only lane 0 of PCIe x2 port to PCIe x1 device. The PCIe Link Training and Status State Machine recognizes the maximum link width both devices support.

0 件の賞賛
返信