T1022 Nor flash erasing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1022 Nor flash erasing

2,092件の閲覧回数
mohsenhaghighat
Contributor III

Hello,

I have T1022 custom board, I want to program the NOR flash for first time, I use hardcoded RCW and codewarrior IDE V10.5 and codewarrior TAP.

 

I make a "Download SRAM" project in codewariior IDE, Then I make a flash programmer target task with 1MHz JTAG clock.
 At first I erase the entire flash, but it errors that " NOT supported", Then I erase one sector of flash, it does not error But it does not complete erasing, in the other words flash erasing is infinity(...) .
Second I blank check the flash, codewarrior does it without no error, because Nor-Flash is not empty, it fails.
Third I program U-boot on the Nor flash, Code warrior does it like erasing, It does not have end, programming the flash is infinity. 
Fourth I verify the Nor flash, Codewarrior does it without no error, But because of mismatches it is failed.
I attach the NOR Flash programmer console and core00_SRAM_DOWNLOAD_T1022 console.
Why does erasing the NOR flash do not complete? Why does programming the NOR flash do not complete? What can I do for this?
Thanks.

Original Attachment has been moved to: core00_SRAM_DOWNLOAD_T1022.txt.zip

Original Attachment has been moved to: flash_programmer_console.txt.zip

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,817件の閲覧回数
ufedor
NXP Employee
NXP Employee

Excuse me, what is the reason to pose question in community if you aready has active Technical Case?

0 件の賞賛
返信

1,817件の閲覧回数
mohsenhaghighat
Contributor III

I think the NXP community and technical case are different places, so I ask here, I do not know, they have a same repliers.

I am sorry about this question, I am appreciative you and your responsibility.

Thanks. 

0 件の賞賛
返信