T1022 Hardcoded RCW codewarrior Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T1022 Hardcoded RCW codewarrior Error

4,665 Views
mohsenhaghighat
Contributor III

Hello,

we design a custom board with T1022 processor and the flash is blank. So we use hardcoded RCW. we connect codewarrior TAP to jtag and try to connecting to CPU.

But it make a error :

"Error: Connect Failed.
Failed to correctly configure the JTAG chain(CCSProtocolPlugin)
Error: Connect Failed."

The switch setting for RCW_SRC is (010011110) , where 0 means ON.

what can I do about it?

Labels (1)
0 Kudos
Reply
11 Replies

4,215 Views
ufedor
NXP Employee
NXP Employee

> where 0 means ON.

Please provide corresponding measured levels of the RCW_SRC signals.

0 Kudos
Reply

4,215 Views
mohsenhaghighat
Contributor III

I measure the voltage of RCW_SRC_SIGNALs. when switch is on the voltage is 0 volt and when switch is off the is 0.7 volt.

0 Kudos
Reply

4,215 Views
ufedor
NXP Employee
NXP Employee

> when switch is on the voltage is 0 volt 

This definitely is incorrect.

Please check that all power supply voltages are properly applied.

0 Kudos
Reply

4,215 Views
mohsenhaghighat
Contributor III

when switch is ON, How much is voltage?

Thanks

0 Kudos
Reply

4,215 Views
ufedor
NXP Employee
NXP Employee

The cfg_rcw_src signals have internal pull-up resistors - refer to the processor's Data Sheet, Table 1. Pinout list by bus:

"4. This pin is a reset configuration pin. It has a weak (~20 kΩ) internal pull-up P-FET that is enabled only when the processor is in its reset state."

0 Kudos
Reply

4,215 Views
dusanferbas
Contributor III

We have similar problems. We designed a board with LS1020A and added pull downs, assuming pull-ups are inside the uP chip. We have a problem with IFC_AD10 when we are booting from SD card. In this case the signal should be high, but we measured 1.2 V, which looks like high, but with 1.8 V logic. Our IFC is designed with 3.3 V logic, which probably qualifies the voltage as low. The solution was to add a 4k7 pull-up.
Does anyone else have such a problem?

We use the MIC826 for a reset, which has a 200 ms period with PORESET- low.
I found the configuration should reside on the IFC bus for 4 clocks after PORESET- goes high.
This seems to be ok.

0 Kudos
Reply

4,215 Views
mohsenhaghighat
Contributor III

Thanks Fedor and Dusan

I add pull up resistors for RCW source near the switch. when siwtch is On the level of voltage is 0.2 Volt and when Switch is off the level of voltage is 1.6 Volt. In this state , some times after reset the PORESET, The HRESET signals still be low(0 volt) and some times it is be high (1.8 volt). when I connect with JTAG when RCW source set to hardcoded, I see two error

1 " Error measuring IR length" 

2 "Failed to correctly configure the JTAG chain"

what can I do for this error?

thanks.

0 Kudos
Reply

4,215 Views
ufedor
NXP Employee
NXP Employee

> I add pull up resistors for RCW source near the switch.

This is incorrect.

It is required to determine why internal pull-up P-FETs do not work properly.

0 Kudos
Reply

4,215 Views
mohsenhaghighat
Contributor III

Do these pull-up P-FETs working with Vcore voltage or OVDd voltage? 

0 Kudos
Reply

4,215 Views
ufedor
NXP Employee
NXP Employee

With OVDD supply voltage.

0 Kudos
Reply

4,215 Views
mohsenhaghighat
Contributor III

I make a mistake when I meaure the RCW source voltage level. I do not reset the board when I measure these.

when board is not reset (HRESET is high) the level voltage of RCW_src is 0 volt (On) and 0.6 volt (off).

But when I reset the board with (PORESET), the voltage level of RCW_src is 0.2 volt(On) and 1.7 volt(off). 

So I delete the pull up resistor near the RCW_src. Still the board is not working

0 Kudos
Reply