T1022 DDR4 DQmaping setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1022 DDR4 DQmaping setup

2,946件の閲覧回数
JohnieSi
Contributor I

 

スポイラ

hello:

      We are having a customized board with T1022 processor,use DDR4 particles MT40A512M16LY-062E,now we want to ifc norflash boot,but now we can‘t boot.we modify uboot added macro definition CONFIG_SYS_FSL_DDR4 and freescale/t104xrdb/ddr.c, source code upload.we use codewarrior QCVS component generate ddr  arguments,then we modify ddr arguments,but now can not bootup,we do not modify DQ maping in QCVS,please help us to solve problem,thanks!

スポイラ
freescale/t104xrdb/ddr.c

 
#include <common.h>
#include <i2c.h>
#include <hwconfig.h>
#include <asm/mmu.h>
#include <fsl_ddr_sdram.h>
#include <fsl_ddr_dimm_params.h>
#include <asm/fsl_law.h>
#include <asm/mpc85xx_gpio.h>
#include "ddr.h"
 
DECLARE_GLOBAL_DATA_PTR;
 
 
void fsl_ddr_board_options(memctl_options_t *popts,
dimm_params_t *pdimm,
unsigned int ctrl_num)
{
const struct board_specific_parameters *pbsp, *pbsp_highest = NULL;
ulong ddr_freq;
 
if (ctrl_num > 1) {
printf("Not supported controller number %d\n", ctrl_num);
return;
}
if (!pdimm->n_ranks)
return;
 
pbsp = udimms[0];
 
/* Get clk_adjust according to the board ddr
* freqency and n_banks specified in board_specific_parameters table.
*/
ddr_freq = get_ddr_freq(0) / 1000000;
while (pbsp->datarate_mhz_high) {
if (pbsp->n_ranks == pdimm->n_ranks &&
    (pdimm->rank_density >> 30) >= pbsp->rank_gb) {
if (ddr_freq <= pbsp->datarate_mhz_high) {
popts->clk_adjust = pbsp->clk_adjust;
popts->wrlvl_start = pbsp->wrlvl_start;
popts->wrlvl_ctl_2 = pbsp->wrlvl_ctl_2;
popts->wrlvl_ctl_3 = pbsp->wrlvl_ctl_3;
goto found;
}
pbsp_highest = pbsp;
}
pbsp++;
}
 
if (pbsp_highest) {
printf("Error: board specific timing not found\n");
printf("for data rate %lu MT/s\n", ddr_freq);
printf("Trying to use the highest speed (%u) parameters\n",
       pbsp_highest->datarate_mhz_high);
popts->clk_adjust = pbsp_highest->clk_adjust;
popts->wrlvl_start = pbsp_highest->wrlvl_start;
popts->wrlvl_ctl_2 = pbsp->wrlvl_ctl_2;
popts->wrlvl_ctl_3 = pbsp->wrlvl_ctl_3;
} else {
panic("DIMM is not supported by this board");
}
found:
debug("Found timing match: n_ranks %d, data rate %d, rank_gb %d\n"
"\tclk_adjust %d, wrlvl_start %d, wrlvl_ctrl_2 0x%x, "
"wrlvl_ctrl_3 0x%x\n",
pbsp->n_ranks, pbsp->datarate_mhz_high, pbsp->rank_gb,
pbsp->clk_adjust, pbsp->wrlvl_start, pbsp->wrlvl_ctl_2,
pbsp->wrlvl_ctl_3);
 
/*
* Factors to consider for half-strength driver enable:
* - number of DIMMs installed
*/
#ifdef CONFIG_SYS_FSL_DDR4
popts->half_strength_driver_enable = 1;
/* optimize cpo for erratum A-009942 */
popts->cpo_sample = 0x59;
#else
popts->half_strength_driver_enable = 0;
#endif
/*
* Write leveling override
*/
popts->wrlvl_override = 1;
popts->wrlvl_sample = 0xf;
 
/*
* rtt and rtt_wr override
*/
popts->rtt_override = 0;
 
/* Enable ZQ calibration */
popts->zq_en = 1;
 
/* DHC_EN =1, ODT = 75 Ohm */
#ifdef CONFIG_SYS_FSL_DDR4
popts->ddr_cdr1 = DDR_CDR1_DHC_EN | DDR_CDR1_ODT(DDR_CDR_ODT_120OHM);
popts->ddr_cdr2 = DDR_CDR2_ODT(DDR_CDR_ODT_120OHM) |
DDR_CDR2_VREF_OVRD(70);       /* Vref = 70% */
#else
popts->ddr_cdr1 = DDR_CDR1_DHC_EN | DDR_CDR1_ODT(DDR_CDR_ODT_75ohm);
popts->ddr_cdr2 = DDR_CDR2_ODT(DDR_CDR_ODT_75ohm);
#endif
}
 
 
 
#define DATARATE_300MHZ        300000000
#define DATARATE_400MHZ        400000000
#define DATARATE_500MHZ        500000000
#define DATARATE_600MHZ        600000000
#define DATARATE_700MHZ        700000000
#define DATARATE_800MHZ        800000000
#define DATARATE_900MHZ        900000000
#define DATARATE_1000MHZ      1000000000
#define DATARATE_1200MHZ      1200000000
#define DATARATE_1300MHZ      1300000000
#define DATARATE_1400MHZ      1400000000
#define DATARATE_1500MHZ      1500000000
#define DATARATE_1600MHZ      1600000000
#define DATARATE_1700MHZ      1700000000
#define DATARATE_1800MHZ      1800000000
#define DATARATE_1900MHZ      1900000000
#define DATARATE_2000MHZ      2000000000
#define DATARATE_2100MHZ      2100000000
#define DATARATE_2200MHZ      2200000000
#define DATARATE_2300MHZ      2300000000
#define DATARATE_2400MHZ      2400000000
 
#define SDRAM_CFG_MEM_EN_MASK       0x80000000
 
/* DDR Controller 1 register values */
#define DDRmc1_CS0_BNDS         0xFF
#define DDRmc1_CS1_BNDS         0x0200023F
#define DDRmc1_CS0_CONFIG       0x80010412
#define DDRmc1_CS1_CONFIG       0x0202
#define DDRmc1_CS0_CONFIG_2     0x00
#define DDRmc1_CS1_CONFIG_2     0x00
#define DDRmc1_CS2_BNDS         0x0240027F
#define DDRmc1_CS3_BNDS         0x028002BF
#define DDRmc1_CS2_CONFIG       0x0202
#define DDRmc1_CS3_CONFIG       0x00010202
#define DDRmc1_CS2_CONFIG_2     0x00
#define DDRmc1_CS3_CONFIG_2     0x00
#define DDRmc1_TIMING_CFG_3         0x01111000
#define DDRmc1_TIMING_CFG_0         0x4055000C
#define DDRmc1_TIMING_CFG_1         0xCCC60E54
#define DDRmc1_TIMING_CFG_2         0x0049111C
#define DDRmc1_SDRAM_CFG        0x05008000
#define DDRmc1_SDRAM_CFG2       0x00401050
#define DDRmc1_MODE_1           0x01010215
#define DDRmc1_MODE_2           0x00
#define DDRmc1_MODE_3           0x00
#define DDRmc1_MODE_4           0x00
#define DDRmc1_MODE_5           0x00
#define DDRmc1_MODE_6           0x00
#define DDRmc1_MODE_7           0x00
#define DDRmc1_MODE_8           0x00
#define DDRmc1_MODE_CONTROL     0x00
#define DDRmc1_INTERVAL         0x18600618
#define DDRmc1_MEM_INIT_VALUE   0xDEADBEEF
#define DDRmc1_CLK_CTRL         0x02800000
#define DDRmc1_INIT_ADDR        0x00
#define DDRmc1_INIT_EXT_ADDR    0x00
#define DDRmc1_TIMING_CFG_4         0x00220001
#define DDRmc1_TIMING_CFG_5         0x05401400
#define DDRmc1_ZQ_CNTL          0x8A090705
#define DDRmc1_WRLVL_CNTL       0x8675F609
#define DDRmc1_WRLVL_CNTL_2     0x00
#define DDRmc1_WRLVL_CNTL_3     0x00
#define DDRmc1_RCW_1            0x00
#define DDRmc1_RCW_2            0x00
#define DDRmc1_CDR_1            0x80040000
#define DDRmc1_CDR_2            0x80040000
#define DDRmc1_SDRAM_CFG_3              0x00
#define DDRmc1_TIMING_CFG_6             0x00
#define DDRmc1_TIMING_CFG_7             0x00
#define DDRmc1_TIMING_CFG_8             0x03115800
#define DDRmc1_DESKEW_CNTL              0x80000000
#define DDRmc1_DQ_MAP0                  0x5B65B658
#define DDRmc1_DQ_MAP1                  0xD96D96D8
#define DDRmc1_DQ_MAP2                  0x5B65B658
#define DDRmc1_DQ_MAP3                  0xD8000000
#define DDRmc1_RCW_3            0x00
#define DDRmc1_RCW_4            0x00
#define DDRmc1_RCW_5            0x00
#define DDRmc1_RCW_6            0x00
#define DDRmc1_MODE_9           0x0500
#define DDRmc1_MODE_10          0x04000000
#define DDRmc1_MODE_11          0x00
#define DDRmc1_MODE_12           0x00
#define DDRmc1_MODE_13           0x00
#define DDRmc1_MODE_14           0x00
#define DDRmc1_MODE_15           0x00
#define DDRmc1_MODE_16           0x00
#define DDRmc1_ERR_DISABLE      0x00
#define DDRmc1_ERR_INT_EN               0x00
#define DDRmc1_ERR_SBE                  0x00010000
 
#ifndef CONFIG_SYS_DDR_RAW_TIMING
fsl_ddr_cfg_regs_t ddr_cfg_regs_1600 = {
.cs[0].bnds = 0x7F,
.cs[1].bnds = 0x008000BF,
.cs[2].bnds = 0x0100013F,
.cs[3].bnds = 0x0140017F,
.cs[0].config = 0x80010422,
.cs[0].config_2 = 0,
.cs[1].config = 0x0202,
.cs[1].config_2 = 0,
.cs[2].config = 0x0202,
.cs[2].config_2 = 0,
.cs[3].config = 0x00010202,
.cs[3].config_2 = 0,
.timing_cfg_3 = 0x02111000,
.timing_cfg_0 = 0x6055000C,
.timing_cfg_1 = 0xB3B40F56,
.timing_cfg_2 = 0x0048D118,
.ddr_sdram_cfg = 0x05008000,
.ddr_sdram_cfg_2 = 0x00401052,
.ddr_sdram_cfg_3 = 0,
.ddr_sdram_mode = 0x01010411,
.ddr_sdram_mode_2 = 0,
.ddr_sdram_mode_3 = 0,
.ddr_sdram_mode_4 = 0,
.ddr_sdram_mode_5 = 0,
.ddr_sdram_mode_6 = 0,
.ddr_sdram_mode_7 = 0,
.ddr_sdram_mode_8 = 0,
.ddr_sdram_mode_9 = 0x0500,
.ddr_sdram_mode_10 = 0x04000000,
.ddr_sdram_mode_11 = 0,
.ddr_sdram_mode_12 = 0,
.ddr_sdram_mode_13 = 0,
.ddr_sdram_mode_14 = 0,
.ddr_sdram_mode_15 = 0,
.ddr_sdram_mode_16 = 0,
.ddr_sdram_interval = 0x18600618,
.ddr_data_init = 0xDEADBEEF,
.ddr_sdram_clk_cntl = 0x02800000,
.ddr_init_addr = 0,
.ddr_init_ext_addr = 0,
.timing_cfg_4 = 0x00220001,
.timing_cfg_5 = 0x05401400,
.timing_cfg_6 = 0,
.timing_cfg_7 = 0x20000000,
.timing_cfg_8 = 0x03114400,
.timing_cfg_9 = 0,
.ddr_zq_cntl = 0x8A090705,
.ddr_wrlvl_cntl = 0x8675F609,
.ddr_wrlvl_cntl_2 = 0x00,
.ddr_wrlvl_cntl_3 = 0x00,
.ddr_sr_cntr = 0x80000000,
.ddr_sdram_rcw_1 = 0,
.ddr_sdram_rcw_2 = 0,
.ddr_cdr1 = 0x80040000,
.ddr_cdr2 = 0x80040000,
.dq_map_0 = 0x00,
.dq_map_1 = 0x00,
.dq_map_2 = 0x00,
.dq_map_3 = 0x00,
//.debug[28] = 0x00700046,
//   .cs[0].bnds = DDRmc1_CS0_BNDS,
//   .cs[1].bnds = DDRmc1_CS1_BNDS,
//   .cs[0].config = DDRmc1_CS0_CONFIG,
//   .cs[1].config = DDRmc1_CS1_CONFIG,
//   .cs[0].config_2 = DDRmc1_CS0_CONFIG_2,
//   .cs[1].config_2 =  DDRmc1_CS1_CONFIG_2,
//   .cs[2].bnds = DDRmc1_CS2_BNDS,
//   .cs[3].bnds = DDRmc1_CS3_BNDS,
//   .cs[2].config = DDRmc1_CS2_CONFIG,
//   .cs[3].config = DDRmc1_CS3_CONFIG,
//   .cs[2].config_2 =  DDRmc1_CS2_CONFIG_2,
//   .cs[3].config_2 =  DDRmc1_CS3_CONFIG_2,
//   .timing_cfg_0 = DDRmc1_TIMING_CFG_0,
//   .timing_cfg_1 = DDRmc1_TIMING_CFG_1,
//   .timing_cfg_2 = DDRmc1_TIMING_CFG_2,
//   .timing_cfg_3 = DDRmc1_TIMING_CFG_3,
//   .timing_cfg_4 = DDRmc1_TIMING_CFG_4,
//   .timing_cfg_5 = DDRmc1_TIMING_CFG_5,
//   .timing_cfg_6 = DDRmc1_TIMING_CFG_6,
//   .timing_cfg_7 = DDRmc1_TIMING_CFG_7,
//   .timing_cfg_8 = DDRmc1_TIMING_CFG_8,
//   .sdram_cfg = DDRmc1_SDRAM_CFG,
//   .sdram_cfg_2 = DDRmc1_SDRAM_CFG2,
//   .sdram_cfg_3 = DDRmc1_SDRAM_CFG_3,// DDRmc1_SDRAM_CFG3
//   .sdram_mode = DDRmc1_MODE_1,
//   .sdram_mode_2 = DDRmc1_MODE_2,
//   .sdram_mode_3 = DDRmc1_MODE_3,
//   .sdram_mode_4 = DDRmc1_MODE_4,
//   .sdram_mode_5 = DDRmc1_MODE_5,
//   .sdram_mode_6 = DDRmc1_MODE_6,
//   .sdram_mode_7 = DDRmc1_MODE_7,
//   .sdram_mode_8 = DDRmc1_MODE_8,
//   .sdram_mode_9 = DDRmc1_MODE_9,
//   .sdram_mode_10 = DDRmc1_MODE_10,
//   .sdram_mode_11 = DDRmc1_MODE_11,
//   .sdram_mode_12 = DDRmc1_MODE_12,
//   .sdram_mode_13 = DDRmc1_MODE_13,
//   .sdram_mode_14 = DDRmc1_MODE_14,
//   .sdram_mode_15 = DDRmc1_MODE_15,
//   .sdram_mode_16 = DDRmc1_MODE_16,
//   .sdram_md_cntl = DDRmc1_MODE_CONTROL,
//   .sdram_interval = DDRmc1_INTERVAL,
//   .sdram_data_init = DDRmc1_MEM_INIT_VALUE,
//   .sdram_clk_cntl = DDRmc1_CLK_CTRL,
//   .init_addr = DDRmc1_INIT_ADDR,
//   .init_ext_addr = DDRmc1_INIT_EXT_ADDR,
//   .ddr_zq_cntl = DDRmc1_ZQ_CNTL,
//   .ddr_wrlvl_cntl = DDRmc1_WRLVL_CNTL,
//   .ddr_wrlvl_cntl_2 = DDRmc1_WRLVL_CNTL_2,
//   .ddr_wrlvl_cntl_3 = DDRmc1_WRLVL_CNTL_3,
//   .ddr_sdram_rcw_1 = DDRmc1_RCW_1,
//   .ddr_sdram_rcw_2 = DDRmc1_RCW_2,
//   .ddr_sdram_rcw_3 = DDRmc1_RCW_3,
//   .ddr_sdram_rcw_4 = DDRmc1_RCW_4,
//   .ddr_sdram_rcw_5 = DDRmc1_RCW_5,
//   .ddr_sdram_rcw_6 = DDRmc1_RCW_6,
//   .deskew_cntl = DDRmc1_DESKEW_CNTL,
//   .ddr_cdr1 = DDRmc1_CDR_1,
//   .ddr_cdr1 = DDRmc1_CDR_2,
//   .err_disable = DDRmc1_ERR_DISABLE,
//   .err_int_en = DDRmc1_ERR_INT_EN,
//   .err_sbe = DDRmc1_ERR_SBE
};
 
fixed_ddr_parm_t fixed_ddr_parm_0[] = {
{1550, 1650, &ddr_cfg_regs_1600},
{0, 0, NULL}
};
#endif
 
 
 
/* DDR model number: MT40A512M8HX-093E */
#ifdef CONFIG_SYS_DDR_RAW_TIMING
dimm_params_t ddr_raw_timing = {
.n_ranks = 1,
.rank_density = 2147483648u,
.capacity = 2147483648u,
.primary_sdram_width = 32,
.ec_sdram_width = 0,
.registered_dimm = 0,
.mirrored_dimm = 0,
.n_row_addr = 15,
.n_col_addr = 10,
.bank_addr_bits = 2,
.bank_group_bits = 2,
.edc_config = 0,
.burst_lengths_bitmask = 0x0c,
 
.tckmin_x_ps = 938,
.tckmax_ps = 1500,
.caslat_x = 0x000DFA00,
.taa_ps = 13500,
.trcd_ps = 13500,
.trp_ps = 13500,
.tras_ps = 33000,
.trc_ps = 46500,
.trfc1_ps = 260000,
.trfc2_ps = 160000,
.trfc4_ps = 110000,
.tfaw_ps = 21000,
.trrds_ps = 3700,
.trrdl_ps = 5300,
.tccdl_ps = 5355,
.refresh_rate_ps = 7800000,
.dq_mapping[0] = 0x0,
.dq_mapping[1] = 0x0,
.dq_mapping[2] = 0x0,
.dq_mapping[3] = 0x0,
.dq_mapping[4] = 0x0,
.dq_mapping[5] = 0x0,
.dq_mapping[6] = 0x0,
.dq_mapping[7] = 0x0,
.dq_mapping[8] = 0x0,
.dq_mapping[9] = 0x0,
.dq_mapping[10] = 0x0,
.dq_mapping[11] = 0x0,
.dq_mapping[12] = 0x0,
.dq_mapping[13] = 0x0,
.dq_mapping[14] = 0x0,
.dq_mapping[15] = 0x0,
.dq_mapping[16] = 0x0,
.dq_mapping[17] = 0x0,
.dq_mapping_ors = 0,
};
 
int fsl_ddr_get_dimm_params(dimm_params_t *pdimm,
    unsigned int controller_number,
    unsigned int dimm_number)
{
static const char dimm_model[] = "Fixed DDR on board";
 
if (((controller_number == 0) && (dimm_number == 0)) ||
    ((controller_number == 1) && (dimm_number == 0))) {
memcpy(pdimm, &ddr_raw_timing, sizeof(dimm_params_t));
memset(pdimm->mpart, 0, sizeof(pdimm->mpart));
memcpy(pdimm->mpart, dimm_model, sizeof(dimm_model) - 1);
}
 
return 0;
}
#else
 
phys_size_t fixed_sdram(void)
{
int i;
char buf[32];
fsl_ddr_cfg_regs_t ddr_cfg_regs;
phys_size_t ddr_size;
ulong ddr_freq, ddr_freq_mhz;
 
ddr_freq = get_ddr_freq(0);
ddr_freq_mhz = ddr_freq / 1000000;
 
printf("Configuring DDR for %s MT/s data rate\n",
       strmhz(buf, ddr_freq));
 
for (i = 0; fixed_ddr_parm_0[i].max_freq > 0; i++) {
if ((ddr_freq_mhz > fixed_ddr_parm_0[i].min_freq) &&
    (ddr_freq_mhz <= fixed_ddr_parm_0[i].max_freq)) {
memcpy(&ddr_cfg_regs,
       fixed_ddr_parm_0[i].ddr_settings,
       sizeof(ddr_cfg_regs));
break;
}
}
 
if (fixed_ddr_parm_0[i].max_freq == 0)
panic("Unsupported DDR data rate %s MT/s data rate\n",
      strmhz(buf, ddr_freq));
 
ddr_size = (phys_size_t)2048 * 1024 * 1024;
fsl_ddr_set_memctl_regs(&ddr_cfg_regs, 0, 0);
 
return ddr_size;
}
#endif
 
 
#if defined(CONFIG_DEEP_SLEEP)
void board_mem_sleep_setup(void)
{
void __iomem *cpld_base = (void *)CONFIG_SYS_CPLD_BASE;
 
/* does not provide HW signals for power management */
clrbits_8(cpld_base + 0x17, 0x40);
/* Disable MCKE isolation */
gpio_set_value(2, 0);
udelay(1);
}
#endif
 
 
phys_size_t initdram(int board_type)
{
phys_size_t dram_size;
puts("swh ddr4 init!\r\n");
dram_size  = fixed_sdram();
#if 0
#if defined(CONFIG_SPL_BUILD) || !defined(CONFIG_RAMBOOT_PBL)
puts("Initializing....using SPD\n");
dram_size = fsl_ddr_sdram();
#else
dram_size =  fsl_ddr_sdram_size();
#endif
#endif
dram_size = setup_ddr_tlbs(dram_size / 0x100000);
dram_size *= 0x100000;
 
#if defined(CONFIG_DEEP_SLEEP) && !defined(CONFIG_SPL_BUILD)
fsl_dp_resume();
#endif
 
return dram_size;
}

 

DQmap.png

ddr41.jpguboot.jpg

 

 

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,945件の閲覧回数
JohnieSi
Contributor I

we do not know how to modify QCVS DDR DQ maping,QCVS DDR other arguments use ddr4 datesheet

0 件の賞賛
返信

2,918件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

If DQ signals are swapped within nibbles, this should be properly set in the DDR_DQ_MAPx registers.

For details, please refer to section "14.4.49 DQ mapping register 0 (DDR_DDR_DQ_MAP0)" in "QorIQ T1040 Reference Manual".

0 件の賞賛
返信

2,894件の閲覧回数
JohnieSi
Contributor I

DDR_DQ_MAPx registers is half-world swapped do not world swapped,my board hardware DDR design most word swapped.such as DQ 7-2-0-5 and DQ 6-3-1-4 right?

0 件の賞賛
返信

2,858件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please use the value addressed in "Table 14-7. Bitfield settings for each byte lane" in T1040RM.

0 件の賞賛
返信

2,914件の閲覧回数
JohnieSi
Contributor I
yes,my board ddr dqmap do not find argument section "14.4.49 DQ mapping register 0 (DDR_DDR_DQ_MAP0)".
please check my board schematic diagram,we dqmap not DQ signals0-3 or DQ signals4-7 swapped,we setup schematic diagram,please tell me how to solve
0 件の賞賛
返信

2,911件の閲覧回数
JohnieSi
Contributor I

dqmap.jpg

0 件の賞賛
返信