Regarding QorIQ ppc SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding QorIQ ppc SDK

1,506 次查看
ronakadesai
Contributor II

At present, there is sdk 1.9 release is out but it is also with kernel version 3.12. For our product we need some features which requires at-least kernel version 3.14 or higher. So, would like to know that is there any plan on releasing SDK 2.0 and if yes, what is the kernel version it will based on?

Also, is there anyways I can have hands on the beta release or pre-release of it ?

标签 (1)
0 项奖励
回复
1 回复

1,399 次查看
bpe
NXP Employee
NXP Employee

SDKs are released twice a year. The upcoming SDK 2.0 will be based on Kernel 4.1.8, planned to be released in May.

For any pre-release version access, approach your FAE or distributor:

Distributor Network|NXP ​


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复