Probability for CPU producing identical data in lockstep architecture?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Probability for CPU producing identical data in lockstep architecture?

1,273 Views
Xingzi
Contributor I

If there is lockstep design to monitor the CPU T2081 output, what is the probability defeating the lockstep mechanism such as producing the identical erroneous data?

For example, if the data size of CPU output is 64 bits, could the probability of 2 CPUs producing the same erroneous data is 1/64*P(CPU0 Error)*P(CPU1 Error)?

The factor 1/data length could be used? Or what is the factor if not?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,256 Views
yipingwang
NXP TechSupport
NXP TechSupport

There are no hardware provisions for that in any T-series or P-series processor and no recommendations for implementing it are available.

0 Kudos
Reply