Issues with External DMA on T1024RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with External DMA on T1024RDB

8,145件の閲覧回数
ehoeg
Contributor I

My team and I are working on setting up Basic Direct External DMA transfers on the T1024RDB.   However, we are thus far unable to successfully setup the external DMA transactions.  Our issue/procedure is as follows:

1. We set up the DMA controller for external control as shown in our code below

2. We initiate a DMA transfer sequence by asserting the DREQ signal from high to low.

3. The MR register responds to the DREQ signal and goes from 0 to 1 (as it should)

4. A DACK signal is generated by the DMA controller

5. DREQ returns to a high state.

6. A DMA transfer occurs from our source address to destination address with the amount of data specified in the BCR register

7. The MR register does not reset back to 0

8. The SR register Programming Error bit is set to 1

9. DREQ asserts back to a low state again to initiate another DMA transfer sequence

10. No DACK signal is generated by the DMA controller and the DREQ signal stays low as a result

According to the T1024RDB reference manual, a programming error can occur as a result of one of the following:

• Transfer started with a byte count of zero

• Stride transfer started with a stride size of zero

• Illegal type, defined by SATRn[SREADTTYPE] and DATRn[DWRITETTYPE],

used for the transfer.

We have our byte count set to a non zero value, striding turned off, and we have tried all the available options for SATRn[SREADTTYPE] and DATRn[DWRITETTYPE] defined in the T1024RDB reference manual.  At this point we are a bit stuck as to what is causing our programming error and preventing further DMA transactions.

Any help would greatly be appreciated.  I have included our setup below:

We first initialize the SATR, SAR, DATR, DAR, and BCR registers.  Then I set the MR0 register.  After setting the MR0 register we cause the DREQ signal to change state from high to low.

RCW:

AA 55 AA 55 01 0E 01 00 08 10 00 0E 00 00 00 00

00 00 00 00 00 00 00 00 4A 80 00 03 80 00 00 12

EC 02 70 00 21 00 00 00 00 00 00 00 00 00 00 00

00 00 00 00 00 07 08 00 00 00 00 00 0B 00 5A 08

00 00 00 00 00 00 00 06 08 13 80 40 55 FA 19 3A

MR0

mrType temp_DMA1_MR0;

temp_DMA1_MR0.bwc = 0x8; // bandwidth sharing

temp_DMA1_MR0.emp_en = 0; // enable external master pause

temp_DMA1_MR0.ems_en = 1; // enable channel from being started by an external DMA start pin

temp_DMA1_MR0.dahts = 0; // 1 byte destination hold transfer size

temp_DMA1_MR0.sahts = 0; // 1 byte source hold transfer size

temp_DMA1_MR0.dahe = 0; // disable destination address hold

temp_DMA1_MR0.sahe = 0; // disable source address hold

temp_DMA1_MR0.srw = 0; // normal operation

temp_DMA1_MR0.eosie = 0; // do not generate an interrupt upon completion of data transfer

temp_DMA1_MR0.eolnie = 0; // do not generate an interrupt upon completion of a list of DMA transfers

temp_DMA1_MR0.eolsie = 0; // do not generate an interrupt upon completion of all DMA transfers

temp_DMA1_MR0.eie = 0; // do not generate an interrupt if a programming or transfer error is detected

temp_DMA1_MR0.xfe = 0; // basic mode - disables striding feature in direct mode

temp_DMA1_MR0.cdsm_swsm = 0; // enable write to source address register to start transfer

temp_DMA1_MR0.ca = 0; // no effect

temp_DMA1_MR0.ctm = 1; // Configure channel for direct mode

temp_DMA1_MR0.cs = 0; // signal set DREQ

temp_DMA1_MR0.cc = 0; // no effect

DMA1_MR0->word = temp_DMA1_MR0.word;

SATR, SAR, DATR, DAR, BCR

unsigned int srceAddrUpper = 0x0;         // Upper Source Address Bits

unsigned int srceAddrLower = 0x80000000;    // Lower Source Address Bits

unsigned int destAddrUpper = 0x0;    // Upper Destination Address Bits

unsigned int destAddrLower = 0x50000000;    // Lower Destination Address Bits

unsigned int byteCount = 256;        // byteCount

// Initialize Source Attribute Register - Channel 0

satrType temp_DMA1_SATR0;

sarType temp_DMA1_SAR0;

temp_DMA1_SATR0.ssme = 0; // disable stride mode

temp_DMA1_SATR0.sreadttype = 0x4; // read, do not snoop local processor

// Initialize Source Address

temp_DMA1_SATR0.esad = srceAddrUpper;

temp_DMA1_SAR0.sad = srceAddrLower;

    // Initialize the Source Address

DMA1_SATR0->word = temp_DMA1_SATR0.word;

DMA1_SAR0->word = temp_DMA1_SAR0.word;

// Initialize Destination Attribute Register - Channel 0

datrType temp_DMA1_DATR0;

darType temp_DMA1_DAR0;

temp_DMA1_DATR0.nlwr = 1; // write without response

temp_DMA1_DATR0.dsme = 0; // disable stride mode

temp_DMA1_DATR0.dwritettype = 0x4; // write, do not snoop local processor

// Initialize Destination Address

temp_DMA1_DATR0.edad = destAddrUpper;

temp_DMA1_DAR0.dad = destAddrLower;

DMA1_DATR0->word = temp_DMA1_DATR0.word;

DMA1_DAR0-> word = temp_DMA1_DAR0.word;

// set byte size

DMA1_BCR0->bc = byteCount;

ラベル(1)
タグ(2)
0 件の賞賛
返信
13 返答(返信)

7,855件の閲覧回数
ehoeg
Contributor I

Our steps and scope captures are attached in the word file.  Thanks.

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

I should mention we have also tried doing an external DMA transfer using the same setup, but changing the source address to the RAM part installed on the T1024RDB.  So our source and destination were both in RAM.  I should mention that we have successfully set up this basic direct DMA transfers (non external) with our setup.  We have only had issues once we started trying to do external DMA transfers.

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try to use MR[BWC]=0x8

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

I have already tried MR[BWC] =0x8 with the same result.  I also have tried different settings stride size and length, and transfer hold size.

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

The issue seems to be connected with the PCIe operation.

Have you also tried MR[BWC] =0x7?

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

Yes, I have tried 0x7 as well as many other sizes in the MR[BWC] register.  I have tried doing DMA transfers from RAM to RAM, so no PCIe in the loop, and I still had the issue.  So I am not sure it is related to PCIe operation.

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please use a digital scope to capture behaviour of DREQ, DACK and DONE signals near the processor's pins and provide the trace for inspection.

How exactly you have reworked the the T1024RDB to use the DMA control signals?

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide the DMA registers dumps:

1) before the transfer

2) after the transfer

What are the source and the destination memories?

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

Hi, here are the register dumps for DMA1 Channel 0

Registers after setting up MR register for external mode, but before asserting DREQ low (before problem)

DMA1_MR0 = 0x09040004

DMA1_SR0 = 0x00000000

DMA1_ECLNDAR0 = 0x00000000

DMA1_CLNDAR0 = 0x00000000

DMA1_SATR0 = 0x00040000

DMA1_SAR0 = 0x80000000

DMA1_DATR0 = 0x40040000

DMA1_DAR0 = 0x50000000

DMA1_BCR0 = 0x00000100

DMA1_ENLNDAR0 = 0x00000000

DMA1_NLNDAR0 = 0x00000000

DMA1_ECLSDAR0 = 0x00000000

DMA1_CLSDAR0 = 0x00000000

DMA1_ENLSDAR0 = 0x00000000

DMA1_NLSDAR0 = 0x00000000

DMA1_SSR0 = 0x00000fff

DMA1_DSR0 = 0x00000fff

Registers after asserting DREQ low (after problem)

DMA1_MR0 = 0x09040005

DMA1_SR0 = 0x00000010

DMA1_ECLNDAR0 = 0x00000000

DMA1_CLNDAR0 = 0x00000000

DMA1_SATR0 = 0x00040000

DMA1_SAR0 = 0x80000100

DMA1_DATR0 = 0x40040000

DMA1_DAR0 = 0x50000100

DMA1_BCR0 = 0x00000000

DMA1_ENLNDAR0 = 0x00000000

DMA1_NLNDAR0 = 0x00000000

DMA1_ECLSDAR0 = 0x00000000

DMA1_CLSDAR0 = 0x00000000

DMA1_ENLSDAR0 = 0x00000000

DMA1_NLSDAR0 = 0x00000000

DMA1_SSR0 = 0x00000fff

DMA1_DSR0 = 0x00000fff

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

What are the source and the destination memories?

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

Sorry about that.

Source Address: 0x80000000

Destination Address: 0x50000000

Transfer Size = 256 bytes

0 件の賞賛
返信

7,855件の閲覧回数
ufedor
NXP Employee
NXP Employee

What are the source and the destination physical memories (interfaces)?

Is the DMA test running on bare board?

0 件の賞賛
返信

7,855件の閲覧回数
ehoeg
Contributor I

Our source destination is RAM on an FPGA connected via PCIe.

Our destination is RAM located on the T1024RDB RAM.

I am not sure exactly what you mean by the DMA test running on bare board, we are using the T1024RDB platform.

0 件の賞賛
返信