Issue Fetching Git Repository for Kernel Build in NXP T2080 QorIQ-SDK-V2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue Fetching Git Repository for Kernel Build in NXP T2080 QorIQ-SDK-V2.0

1,638 Views
thenveer
Contributor I

 

Dear NXP Support Team,

I am currently working with the NXP T2080 QorIQ-SDK-V2.0-20160527-yocto SDK. While building the SDK, I encountered the following error:

host@39abc714f735:~/QorIQ-SDK-V2.0-20160527-yocto/build_t2080qds$ bitbake fsl-image-minimal
Loading cache: 100% |#######################################################################################################################################################################| ETA: 00:00:00
Loaded 6083 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "powerpc-fsl-linux"
MACHINE = "t2080qds"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "m32 fpu-hard e6500 altivec"
TARGET_FPU = "hard"
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-nxp-npi-1703 = "jethro-sdk-v2.0-ga-17.03:d8f8d3a5d3ee18f881466938b847cef9b08c4a35"

NOTE: Preparing RunQueue
NOTE: Checking sstate mirror object availability (for 8 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://git.freescale.com/ppc/sdk/linux.git;nobranch=1, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/home/thenveer/QorIQ-SDK-V2.0-20160527-yocto/downloads/git2/git.freescale.com.ppc.sdk.linux.git'...
fatal: unable to connect to git.freescale.com:
git.freescale.com[0: 54.179.117.50]: errno=Connection timed out


ERROR: Function failed: Fetcher failure for URL: 'git://git.freescale.com/ppc/sdk/linux.git;nobranch=1'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/thenveer/QorIQ-SDK-V2.0-20160527-yocto/build_t2080qds/tmp/work/t2080qds-fsl-linux/linux-qoriq/4.1-r0/temp/log.do_fetch.1993207
ERROR: Task 4 (/home/thenveer/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 472 tasks of which 470 didn't need to be rerun and 1 failed.
No currently running tasks (425 of 491)

Summary: 1 task failed:
/home/host/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.


This issue is preventing me from proceeding with the build. Could you kindly provide guidance or suggest a workaround to resolve this issue and complete the SDK build?

For your reference, here are the details of my environment:

  • SDK Version: QorIQ-SDK-V2.0-20160527-yocto

  • Machine: t2080qds

Any assistance in resolving this would be greatly appreciated.

 

 

0 Kudos
Reply
4 Replies

1,575 Views
yipingwang
NXP TechSupport
NXP TechSupport

In recipe sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb, SRC_URI should be defined as the following.

SRC_URI = "git://git.freescale.com/ppc/sdk/linux.git;branch=sdk-v2.0.x"

SRCREV = "bd51baffc04ecc73f933aee1c3a37c8b44b889a7"

0 Kudos
Reply

1,569 Views
thenveer
Contributor I
Yes, the SRC_URI in the source file sources/meta-freescale/recipes-kernel/linux/linux-qoriq_4.1.bb is defined exactly as you mentioned:

SRC_URI = "git://git.freescale.com/ppc/sdk/linux.git;branch=sdk-v2.0.x"
SRCREV = "bd51baffc04ecc73f933aee1c3a37c8b44b889a7"


However, when I checked git.freescale.com, I was unable to locate the repository as it seems to be inactive or no longer available.

Could you please confirm if there is any patch file or updated repository for the latest source? If the repository is no longer available, could you guide me on the alternative source or replacement from where we should fetch the kernel?

Your guidance on this would be much appreciated.

0 Kudos
Reply

1,506 Views
yipingwang
NXP TechSupport
NXP TechSupport

I did verification on my Linux PC, there is no problem to get Linux Kernel source code.

I installed ISOs "QorIQ Linux SDK v2.0 SOURCE.iso" and "QorIQ Linux SDK v2.0-1703.tar.bz2", then run the following commands to get Linux Kernel source code successfully.

$ source ./fsl-setup-env -m t2080qds

$ bitbake virtual/kernel -c patch -f

 

The source code tar balls are provided in the SOURCE ISO, no need to download them from the networking. Did you touch "downloads" folder in the installation folder? Please check whether "downloads/git2/git.freescale.com.ppc.sdk.linux.git" exist?

Please remove your current installation folder and install "QorIQ Linux SDK v2.0 SOURCE.iso" and "QorIQ Linux SDK v2.0-1703.tar.bz2" again.

0 Kudos
Reply

1,492 Views
thenveer
Contributor I

Thanks for the input. I am now able to build the SDK successfully.

I have one additional query:
What changes are required in this SDK to configure both PCIe controllers to operate as Root Complex?

thenveer_0-1769076406919.png

 

0 Kudos
Reply