INTLVEN for T1040RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

INTLVEN for T1040RDB

1,560件の閲覧回数
hv
Contributor II

I found in the P4080RM the ability to interleave SRAM address space by setting CPCSRCR0[INTLVEN] bit.  But the INTLVEN bit is not defined in the T1040RM.  Does that mean I can't interleave SRAM in the T1040?  Thanks!

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,448件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Interleaving may be used only if you have two CPC sram memories. In case of P4080 there are two CPC blocks, but in T1040 there is only one CPC block, so there is nothing to interleave with.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,448件の閲覧回数
hv
Contributor II

Thanks!

0 件の賞賛
返信