Does T4240QDS development/test board support Display?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does T4240QDS development/test board support Display?

1,552件の閲覧回数
A-R
Contributor II

Hi,

I'm going through schematic and Layout of T4240QDS development/test board and I can't find any display support on  T4240QDS development/test board. I want to connect display with this board to use it as normal PC. Can anyone tell me how can I connect display with this board and through which port or component I can do that?

Also I noticed that there is no GPU support available on board. Do I have to connect some GPU for display as well with that board?

0 件の賞賛
返信
2 返答(返信)

1,540件の閲覧回数
A-R
Contributor II

@ufedor Thanks for your reply. I want to ask some more questions as well.

I went through T1040 which have DIU. Now can I use that processor for GUI based Linux? And also is there any reference design available of that processor with Display/VGA/HDMI? 

I'm looking for any NXP processor on which I can do some processing using GUI based Linux. Can you recommend any processor with it's reference design? It will be very helpful for me. 

 

Thanks in advance. 

0 件の賞賛
返信

1,543件の閲覧回数
ufedor
NXP Employee
NXP Employee

T4240QDS does not possess a display port.

UART COM port is used for communication with a host PC.

Technically, a PCIe graphics card can be inserted into an on-board PCIe slot, but there is no such reference solution from NXP.

0 件の賞賛
返信