Could not connect to probe(or other debug links). CC string is invalid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Could not connect to probe(or other debug links). CC string is invalid

3,717 Views
athershehzad
Contributor III

I am trying to flash my T1042RDB based custom board using Code warrior tap. When I connect my codewarrior tap to my PC, Green LED starts blinking that shows the connectivity of PC and Codewarrior tap. I am also able to see my freescale probe in device manager but it is not shown in the notification tray. When I starts flashing, it gives the error that

Connection failed.

Could not connect to probe [or other debug link]. CC string is invalid.

What might the reason for this error ?

Labels (1)
Tags (2)
0 Kudos
Reply
6 Replies

3,470 Views
athershehzad
Contributor III

Sir Is there any other way by which I can configure my Codewarrior Tap by myself ?

0 Kudos
Reply

3,470 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ather Shehzad,

The problem should be caused by the unstable hardware, please return it for a new TAP.

Thanks,

Yiping

0 Kudos
Reply

3,466 Views
athershehzad
Contributor III

Thanks Yiping Wang
You might be right because when I enter show cc it gives me error
0: USB open failure

but sometimes it gives me the expected result

0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

Yes Code warrior is shown in device manger that can be seen in the attachment below

What is the solution to the usb connection issue ?

Regards

0 Kudos
Reply

3,466 Views
yipingwang
NXP TechSupport
NXP TechSupport

It's seems that the hardware of your CodeWarrior TAP is not stable, please contact your local FAE to return and replace it with new one.

0 Kudos
Reply

3,466 Views
athershehzad
Contributor III

Is there any other way to configure the CodeWarrior hardware by ourself ?

Regards,

0 Kudos
Reply

3,464 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ather Shehzad,

It seems that there is problem to detect CodeWarrior TAP with USB connection.

Please open CodeWarrior Connection Sever to check whether CodeWarrior information can be returned correctly.

(bin) 2 % config cc cwtap
(bin) 3 % show cc
0: CodeWarrior TAP (cwtap) CC software ver. {0.0}

In addition, please check whether CodeWarrior TAP can be detected as the attachment from the device manager.

Thanks,

Yiping

0 Kudos
Reply