Component DDR4 Schematic?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Component DDR4 Schematic?

跳至解决方案
3,487 次查看
trevorfox
Contributor III

Hi

I'm having trouble getting this T1042 custom board to work. It uses component DDR4 (instead of DIMM which Dev Board uses) and I want some type of known functional hookup to compare it to.

As I said, the T1042D4RDBDev Board uses DIMM so I can't easily use that one and DIMMs have different functionality than component.

0 项奖励
回复
1 解答
3,452 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

在原帖中查看解决方案

2 回复数
3,453 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Attached a page with the LS1043A processor and 32-bit DDR4 interface. 64-bit interface uses the same idea and upper-numerated signals.

3,427 次查看
trevorfox
Contributor III

Thank you very much!

0 项奖励
回复