CPU up timeout. SMP not working randomly(Processor 2 is stuck) in linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CPU up timeout. SMP not working randomly(Processor 2 is stuck) in linux

3,110件の閲覧回数
karunakaranradh
Contributor IV

In U-Boot, "CPU up timeout . CPU up mask is 1 should be f" printed randomly,  If CPU up timeout in U-Boot, after that kernel throw the below error.

Processor 2 is stuck.
smp_85xx_kick_cpu: Can not start CPU #3. Start CPU #2 first.
smp: failed starting cpu 3 (rc -2)
Processor 4 is stuck.
smp_85xx_kick_cpu: Can not start CPU #5. Start CPU #4 first.
smp: failed starting cpu 5 (rc -2)
Processor 6 is stuck.
smp_85xx_kick_cpu: Can not start CPU #7. Start CPU #6 first.
smp: failed starting cpu 7 (rc -2).


This CPU up timeout  error occurred randomly at any time.

Kindly suggest us to resolve this issue.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,700件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Karunakaran Radhakrishnan,

Under u-boot prompt, please use the command "cpu <num> status" to check whether the stuck processor is running.

If the CPU doesn't run, please check the probable hardware cause.

Core power supply failure       

Improper processor connection, please refer to the design checklist which could be downloaded from NXP public Website.

Incorrect timing of POR configuration signal(s), please refer to Power on reset initialization section in the processor reference manual.

If processors run normally, please check DDR memory, please enable "mtest" in u-boot to do more test on DDR memory.

If you have CodeWarrior+CodeWarrior TAP, you could refer to Debugging Linux Kernel with CodeWarrior for PA to debug Linux Kernel to get the exact information.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,700件の閲覧回数
chengdang
Contributor I

Hi,

I am facing same issue. For me processor 1 is stuck and linux kernel was not booting after that. Have you resolved this issue and how.

0 件の賞賛
返信