Accessing GPIO in QorIQ u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Accessing GPIO in QorIQ u-boot

1,264 次查看
kylevonschmacht
Contributor I

To whom it may concern,

We're using a custom board using the T2081, derived from the T2080RDB and the T1042RDB.

We find ourselves needing to use a GPIO during the u-boot phase.

To that end:

-What do we need to include in the build?

-What configurations and #define are needed?

-What custom code do we need to generate to fill in the gaps?

Thanks for your help,

Kyle

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,036 次查看
Pavel
NXP Employee
NXP Employee

There is no GPIO driver in u-boot for QorIQ processors, but u-boot driver structure is relatively simple, so you can create your own GPIO driver using other GPIO drivers as reference. For example drivers please look /drivers/gpio/ folder in U-boot sources folder.

Use as example the mpc85xxx_gpio.c file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复