32GB NAND memory configuration in T2080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32GB NAND memory configuration in T2080

1,268件の閲覧回数
vidyasagartata
Contributor II

We are using using NAND part number MT29F256G08CMCBBH2, we have configured all CS properly but read/write do not happen.

Getting error in the u-boot

 

NAND:  fsl_ifc_cmdfunc: error, Default unsupported command 0x5.
fsl_ifc_read_buf beyond end of buffer (48 requested, 0 available)
fsl_ifc_cmdfunc: error, Default unsupported command 0x5.
fsl_ifc_read_buf beyond end of buffer (48 requested, 0 available)
fsl_ifc_cmdfunc: error, Default unsupported command 0x5.
fsl_ifc_read_buf beyond end of buffer (48 requested, 0 available)
fsl_ifc_cmdfunc: error, Default unsupported command 0x5.
fsl_ifc_read_buf beyond end of buffer (48 requested, 0 available)
32768 MiB

 

I am using T2080 processor with SDK2.0.

Please let me know how this problem will get resolve.

Thanks,

Vidya

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,006件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the following pages:

https://www.google.ru/url?sa=t&rct=j&q=&esrc=s&source=web&cd=7&cad=rja&uact=8&ved=0ahUKEwit-N3S3bXVA...

 

https://community.nxp.com/docs/DOC-333350?commentID=45404


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信